2015-04-24 02:09 PM
Hello everyone, I have a project which i want to add the network capabilities . I am using the SMT324x9I-Eval board to do my first test with the project LwIP_TCP_Echo_Client included in STM32F4Cube 1.5.0.
I am absolutely not able to get a packet from the board on my PC.I have downloaded EchoTool application and run it on my PC. In my project I have changed the IP destination to 10.0.0.11 , my source to 10.0.0.10 and put my gateway to 10.0.0.11.The link in between is a cross-over cable directly into a 2nd network card. I am using Wireshark to monitor the NIC and I don't see any pack going in. Naturally, the echo tool server doesn't get any request.Anyone has experienced with this demo application or network API on this evaluation board.Regards, #smt32f4x9i-eval-ethernet-lwip