2019-02-13 05:01 AM
My device use STM32L0 controller and Hal USB Device CDC class is implemented in it. When connected to Windows 10 OS the "Device description request Failed" message is shown. But on updated windows 10 OS it is working fine as it should. So is there any way to make it work in non updated Windows 10 ???
2019-02-13 04:18 PM
Which win10 version is NOT updated? and which is updated?
-- pa
2019-02-13 04:38 PM
It's a pretty hefty lift to fix microsoft's broken mess, especially if you aren't letting it fix itself or to pull current drivers.
2019-02-13 09:56 PM
Non Updated windows 10 (Device not recognized) Info:
Edition - Windows 10 Home
Version - 1803
Updated working Windows 10 info:
Edition - Windows 10 Pro
Version - 1803