cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Thread Safe Solution for Makefile Projects

cvanbeek
Associate III

I have a Makefile project for an STM32L4 using FreeRTOS that I started with STM32CubeMx. I'm trying to enable one of the Thread-Safe strategies for FreeRTOS. I have tried both strategy #4 and #5, but both of them jump to the error handler on the `STM32_LOCK_BLOCK_IF_NULL_ARGUMENT` check in the `__retarget_lock_acquire_recursive` function in `newlib_lock_glue.c`

It doesn't seem like the locks are being initialized in the Makefile project. Is there any additional setup needed for thread safe implementations of a Makefile project? Otherwise, are there any additional flags that I need to send to gcc (or any of the other arm-none-eabi tools)?

Best regards,

Cory

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
cvanbeek
Associate III

For anyone else having this issue, it was resolved by upgrading my arm-none-eabi build tools from version 11.3 to version 12.2.

What does this mean? The newlib (nano) built differently in these versions?