2018-06-03 10:44 AM
Hello. I am developing the device on STM32L433 with the following logic of operation:
1) Pressed the button - the sensors are reading (SPI, I2C), data from them are written to the memory card via SDIO + FatFS2) Pressed the button again - recording stops, the device can be connected to USB as a MSC and copy the previously recorded data.The bundle of SDIO + FatFS is working, the data is normally written, but MSC does not work at all. If I am add the line HAL_SD_Init (& hsd1) to the static void function MX_SDMMC1_SD_Init (void), the card is normally detected and works, but after that FatFS stops working on the controller. How to merge them together so they do not conflict?#sdio #usb-msc #fatfs2018-08-12 6:44 AM
I have the same problem using a STM32F446RETx.
I can configure CubeMX with USB_Device, Mass Storage Class with USB_OTG_FS and Device_Only and I can read/write the contents of the SD card through the PC.
If I add FATFS with SD Card, I can read/write the contents of the SD card with FatFs but cannot open the SD Card with the PC. I get an error saying I need to format the card.