cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 MCU's with 10/100 Ethernet MII/RMII module

MCUpwr
Associate III

Does ST have list of STM32 MCU's with 10/100 Ethernet MII/RMII module? Also does ST have an MCU's with 10/100 Ethernet MII/RMII module in 64 pin package.I know for STM32F207xx series 100 pin package.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

There is a complete list of all STM32 in the Developer Zone, which you can filter e.g. by Ethernet.

The list of STM32 with 10/100 Ethernet is just too long to include here, but just try it yourself online.

Hope that helps?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

There is a complete list of all STM32 in the Developer Zone, which you can filter e.g. by Ethernet.

The list of STM32 with 10/100 Ethernet is just too long to include here, but just try it yourself online.

Hope that helps?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MCUpwr
Associate III

Thanks.

You're welcome!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.