2019-12-25 1:39 AM
Hi,
I currently working on a USB PD project. I am quite interested in ST solution. I need a DRP, dual power role, features so STUSB1602 should be included in the design. I just found the application firmware is developed based on STM32F071RB and the system is running in FreeRTOS. I can modify the application firmware in the nucleo demo board.
I would like to choose a smaller MCU which is compatible to the STM32F071RB. I targeted the STM32F071CB 48 pins UFQFPN.
My question is can I directly flash the STM32F071RB firmware to STM32F071CB?
Thank you very much