STM32 - bootloader commands for readout protect/unprotect not working...?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-04 2:35 PM
I am working with several STM32, let's focus on the STM32L4P5. I wrote a windows utility which does a nice job of loading code with the bootloader, per the AN3155 documentation. It is nicely robust, and I've been using it for a couple months. I want to add the capability of selecting to protect or unprotect readout with a user selection.
I send the 0x92+0x6D to unprotect, then write the code, and the code executes just fine, but hooking up the J-link re-erases everything, indicative of protection being set.
Has anybody used this successfully?
- Labels:
-
Bootloader
-
Documentation
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-05 3:49 AM
Try check if this work with stm32CubeProgrammer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-05 10:54 AM
No. I'm not using Cube. I have a product with several embedded STM32 micros, and I need to be able to reprogram any of them via a single USB port. I need to use the bootloader, and I need custom code to do this so that I can use the micro riding on the USB UART to pass-thru as appropriate and wiggle BOOT0 and \RESET of the downstream boards as appropriate. This should work according to the documentation --- all the other functions work great and the bootloader functions. I just can't set the read unprotect.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-05 9:53 PM