2017-10-13 1:19 PM
Hi,
I have recently purchased a number of NUCLEO-L476 boards but cannot get the USB drivers to install correctly whch are required for both ther STLINK utility and also for System Workbench for STM32.
I am using a Windows 10 64-bit laptop with USB 3 ports and have installed the STLINK utility, en_stsw-link004.zip, which includes the relevent USB drivers. The installation appears to succeed, however, when I plug in the development board via USB Windows complains with 'USB device not recognised'. In Device Manager, under the Universal Serial Bus controllers section I have an entry which shows as 'Unknown USB Device (Device Descriptor Request Failed), which is presumably the STLINK/V2 probe in the development board. Also I have no virtaul COM port entry.
I have tried the same on a Windows XP and Windows 7 PC and all report similar errors. Its as if the development board is not compatible with the driver or the driver has a problem.
I have searched the internet and this forum and I am completely out of ideas to try next.
According to the Getting Started card in the box an LED should flash, and when a button is pressed it changes. I am getting no flashing LED at all. Also the power LD3 is not on either. LD1 on the probe does, however, flash 3 or 4 times when it is plugged into the USB port. I am certain that the links specified on the card are configured correctly.
Any help would be appreciated.
Regards
FarmerJo
#stm32l476 #stm32 #stm32-usb-driverSolved! Go to Solution.
2017-10-21 1:55 AM
Hi Imen D,
Having tried many things including your suggestion it turned out to be a faulty USB cable. The cable was new about six months ago and one of many I had knocking about. Trust me to use the only one that was broken.
Thanks for yout reply.
Regards
FarmerJo
2017-10-20 9:15 AM
Hello,
Try to upgrade firmware version using STM32 ST-LINK Utility: go to ST-LINK > firmware update, or through this Link
http://www.st.com/en/development-tools/stsw-link009.html
Best Regards
Imen
2017-10-21 1:55 AM
Hi Imen D,
Having tried many things including your suggestion it turned out to be a faulty USB cable. The cable was new about six months ago and one of many I had knocking about. Trust me to use the only one that was broken.
Thanks for yout reply.
Regards
FarmerJo
2019-01-18 2:29 PM
Hello Imen,
Just for you to know, it's impossible to upgrade the firmware when the PC don't even recognize the USB device.
Regards,
Luis Padierna
2019-01-18 2:33 PM
I had exactly same problem but with an ST-LINK V2 standalone. I realized the problem was using the ST's official USB cable, the solution is to use a USB cabe that actually works. For me as soon as I changed the cable, the problem was solved.
2020-08-08 3:51 AM
Hello, I am experiencing the same issue with the STM32MP157C-EV1 ST-Link v2.1 on both Windows 10 64-bit and Ubuntu 18.04. I tried multiple USB cables and none of them works, there is the same entry in device manager on Windows stating it can not obtain device descriptor (code 43). I used the same cable(s) for the DK2 and it had no issue connecting, ST-Link was recognized right away. I believe all drivers are installed properly as DK2 is recognized. Is the board faulty or there is a way to fix this?