cancel
Showing results for 
Search instead for 
Did you mean: 

STL Flash test failed

MauroM
Associate

Hello,

I'm working to add the STL Library to my existing project, I'm trying to run the function StlSingleTest but it fails (STL_FAILS) executing the STL_SCH_RunFlashTM(&StlFlashStatus) section.

micro: STM32F446ZET

Flash:

Bootloader: 0x08000000 - 0x0800FFFF

App: 0x08010000 - 0x0807FFF

The StlSingleTest is called from the APP,

config file (stl_user_param_template.c) 

STL_ROM_START_ADDR (0x08010000UL)

STL_ROM_END_ADDR (0x0807FFFFUL)

TEST_FLASH_SECTION_NB 4

Can someone help me?

Thank you in advance.

Mauro

 

3 REPLIES 3

These materials under NDA, work with your FAE. Or open an online support request

https://community.st.com/t5/stm32-mcus-other-solutions/running-into-a-strange-problem-we-re-working-on-a-safety-project/td-p/153442

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Petr Sladecek
ST Employee

Hello,

it is not clear which safety STL library is your target. Is it X-CUBE-STL or X-CUBE-CLASSB?

Anyway I suggest to verify if all the preconditions described at chapter Flash memory tests are applied and if each memory section applied for the test has its CRC image stored at proper place at the CRC area.

Best regards,

Petr

PavelSingh
Associate

Hello Mauro,

I am facing a similar issue.

Would your problem solved, please share your experience.

Kind regards,

Pavel