cancel
Showing results for 
Search instead for 
Did you mean: 

static/DHCP networking with LWIP

alanb
Associate II

I generally want to support both static/auto/dhcp in software config. This is most easily done by changing LWIP.c

Around line 62:

 

/* IP addresses initialization with DHCP (IPv4) */ ipaddr.addr = gstate.ipaddr; // NOT 0 netmask.addr = gstate.netmask; // NOT 0 gw.addr = gstate.gwaddr; // NOT 0

 

Around 92

 

if (gstate.dhcp) { dhcp_start(&gnetif); } else { ipaddr.addr = gstate.ipaddr; netmask.addr = gstate.netmask; gw.addr = gstate.gwaddr; dhcp_stop(&gnetif); netif_set_down(&gnetif); netif_set_addr(&gnetif, &ipaddr, &netmask, &gw); if (netif_is_link_up(&gnetif)) { /* When the netif is fully configured this function must be called */ netif_set_up(&gnetif); } }

 

However such changed keep getting trampled on by code generation when I update STM32Cube. Is there any way to protect changes so they don't get overwritten?

I appreciate that to support either Static or DHCP this is a config option in the code generator, but I generally want to support everything I can!

Alan

3 REPLIES 3
Pavel A.
Super User

A good idea, but should be more or less easy to do this with the "user code areas"  and ifdefs.

 

It _so nearly_ is, but unfortunately the call to 

 dhcp_start(&gnetif);

is just before the /* USER CODE BEGIN 3 */

block which makes it hard to bypass and the init of ipaddr/netmask/gwneeds to be done before this and there isn't a user code block available.

 

Alan

 

// something like this ... #ifdef USE_STATIC #define dhcp_start(x) /*nothing*/ #endif