2018-10-31 8:15 AM
2018-10-31 8:56 AM
Sounds like a homework problem.
Review the HID Host examples for the specific STM32 you're using, probably a few hundred parts from different families, so you might want to narrow that down a little.
The Cube downloads for assorted families unpack with large example trees, for assorted boards, including HID examples.
2018-10-31 8:59 AM
Ok, duplicate thread, stick to your first one
Work with your teachers and colleagues.
2018-10-31 9:02 AM
Consider using a NUCLEO-F429ZI, the F4 supports HOST operation, and has a HID example..
STM32Cube_FW_F4_V1.21.0\Projects\STM32F429ZI-Nucleo\Applications\USB_Host\HID_Standalone
2018-11-01 3:06 AM
Sir I have completed all process. But i do not know which class or structure is use from library function. My means what is type of variable which store specific key press data of USB keyboard.please give me your suggestion to set this problem. thank you
2018-11-02 9:32 PM
thank you very much sir. you had provided me link to answer my question but i did not understand at that time.Thank you so much sir