2023-08-26 01:10 AM
Hi,
I have a problem with SBSFU.
I'm using STM32G0B1RE dev kit.
But I have got STM32G071RB example. G071RB is example works fine in G0B1RE board.
The problem occurs when I change Compile Symbol to STM32G0B1xx STM32CubeIde Properties > Settings > GCC Compiler > Symbol to STM32G0B1xx
SBSFU failed to download the .sfu file on the second time after erasing the 32bytes header from example. It throws Flash error after during hearder signature verification.
I need to change symbols to STM32G0B1XX to implement USB CDC code instead UART.
TIA
2023-08-29 03:43 PM
Hello @Tarun ,
The flash error encountered while verifying the signature and may be captured during an installation procedure.
I recommend you check the UM2262 which contains all steps and detailed. The Table 6 lists the main error messages with their explanation.
Imen
2023-08-30 01:55 AM
Hi Imen,
Thank you for your reply. I understand that Flash error causing during installation procedure. The question is why it was failed when I change symbol to STM32G0B1xx. Though I change symbol, able to download application first time and download failed when I corrupt the signature from tests provided by ST example code? The same code download working with STM32G071xx symbol before and after signature corruption. Could you please elaborate the answer where I need to focus?