2025-01-30 1:27 PM
Hi,
when I increase the size of the ThreadX trace buffer above 30k the RTT output is not working anymore (Below 30k RTT works fine).
static uint8_t trace_buffer[1024*64] __attribute__((section(".trace")));
My guess is that the RTT viewer can't find the RTT control block anymore. I can't explain myself why this is the case.
When checking the map file I find the control block near the end of SRAM1, which should not be a problem I think?
Anyone some idea, how to fix the RTT output? Any help is appreciated :)
Thank you
Regards
John
Solved! Go to Solution.
2025-01-31 12:56 AM
After setting the address of the control block in the RTT viewer the output works again.
2025-01-31 12:56 AM
After setting the address of the control block in the RTT viewer the output works again.
2025-01-31 1:03 AM
@WhoIsJohnGalt wrote:My guess is that the RTT viewer can't find the RTT control block anymore.
That would be something to take up with Segger: