Problem with firmware package and P-L496G-CELL01 board. why C2C device not connect ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-18 2:44 AM
hii,
I have just started working on P-l496g-cell01 board and download the packages from st web site.
I use en.x-cube-cloud-gen packages in which default code is available to connect grove stream cloud. I follow all steps and also check all jumper all are properly connected but when i debug the code at the stage of initialization of UG96 Cellular device not connect and show the error on tera term "Trying to connect with the embedded SIM
Fail to AT SYNC, after several attempts
C2C AT comunication error with the C2C device
C2C device might be disconnected or wrongly connected
Error initializing the module!" please help me how to solve this error ?
C2C device connect proper way power led ON and also connect with the NW my Esim also activated.
Thank you,
Regards,
sadik pinjari.
- Labels:
-
STM32CubeExpansion
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-18 2:50 AM
embedded SIM = soldered SIM on board with the modem.
Did you activate the eSIM on the C2C portal?
Otherwise, it is possible to insert a MicroSIM which needs to be selected in the code (probably a #define).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-18 2:52 AM
found this video :
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-18 3:11 AM
Thanks for your reply.
yes i active sim and also check on emnify site status is activated.
I see this video and follow all steps strictly first time device connected and also i turn on and off led. But than after 2nd time i reset the board and try again than error is
" AT<CR>
ATCore:TIMEOUT EVENT(3000 ms)
UG96 ERROR:Impossible to sync with modem
ATParser ERROR:parser f_getCmd error
ATCore ERROR:AT_sendcmd error: get at command
ATCore ERROR:AT_sendcmd error: process AT transaction
CS ERROR:<Cellular_Service> error during HW device reset
=== CST_reset_modem_mngt Fail !!! ===
=== CST_set_fail_state - 2 !!! ==="
please help me i m stuck from yesterday.
Thanks in advance.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-18 3:58 AM
Looks like the modem is not responding.
If you still have the original discovery MCU SW code inside, it will power up the modem and the modem LED will turn on.
Then, using a windows PC and connect it to the modem USB port, you can use Quectel Qnavigator to manually test the modem/sim/connectivity alone
https://www.bqtek.com/en/download/qnavigator_1_4.zip
Seems to be on-line Quectel tool for modems.
Until an ST guy reply to this forum, this can help you move forward.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-18 4:45 AM
Thanks for the reply.
yes, right it modem responding problem MCU sent the "AT" commend but not receive "ok" or any data from modem.
I check some commends to modem port it's responding all commend but when i connect with MCU and debug than it's not work don't know why ?
if someone face this type of issue please help.
any little help appreciated.
Thanks in advance.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-18 4:53 AM
Have you tried the demo binaries from the C2C site, or are you currently compiling a project?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-18 5:08 AM
yes. i first try binaries file which is available on on C2C site but only once it works and shows error so i found en-x-cube-cellular packages which is available on st site and try to compile. but it's not work. i also install Qnevigator as u suggest and debug it give response +CPIN: READY, +QIND: SMS DONE, +QIND: PB DONE
this are the last commond send by the module than it shows error
"Fail to AT SYNC, after several attempts
C2C AT comunication error with the C2C device
C2C device might be disconnected or wrongly connected
Error initializing the module! "
please help if possible.
Thanks for giving your time .
,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-25 4:59 AM
problem solved,
It's Baud rate and hardware flow control configuration problem now module working properly.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-07 9:33 PM
Hi shaikh,
i am getting the same error,can you please elabrote how did you solve the issue,did yo u change anything in the code iam also using firmware package and P-L496G-CELL01
DIJITH P