2017-01-23 12:37 AM
Hello everyone,
I am trying to download the F7 firmware package using this link :
but the download doesn't want to start... (it's working for other firmware like Cube F0, F4....)
Does some of you have working link ? Or an older working version ? Am I the only one with this issue ^^' ?
Thank you in advance, and have a good day !
Pierre
#download #unfitforpurpose #stm32cubef7 #firmware2017-01-23 05:29 PM
There does appear to be something gravely wrong with the world facing side of your server. Different ISP with a 3MByte/s download still chokes midway through the file, on both Firefox and Chrome.
You need to look at the logs and see all the failed downloads. You need to consider the value of the login/download method and if there is a timeout or data limit, and if HTTP is appropriate for 500MB-1GB files which isn't a protocol supporting a restart. Consider BitTorrent?
2017-01-23 10:38 PM
Hello Madam,
This link stm32cube f7 still has problem,i try to download from google chrome and Microsoft edge ,but download not start.
2017-01-24 12:21 AM
I managed to download it through CubeMX. I've uploaded the library to dropbox if that helps anyone:
https://www.dropbox.com/s/fh42ryqp0uwfu3b/stm32cube_fw_f7_v160.zip?dl=0
2017-01-24 05:36 AM
Thanks Alex,
Finally i download stmcubef7 from link provide by you.
2017-01-24 08:45 AM
It takes a long time to start, and repeatedly chokes at around 350-370MB, tried close to a dozen times on different systems, browsers and ISP
It is a pretty sorry state of affairs when a web server can't perform the basic task of providing a file for download, and all the unnecessary scripts, redirects, authentication!!
♯
2017-01-25 02:47 AM
Dear Users,
Issue has been identified and it is now fixed.
Sorry for the inconvenience it may bring.
Regards
Imen
2017-03-31 12:43 PM
Hi all
I have also problem with download STM32Cube F7 v 1.6.0 Maybe anyone have others link ? The Drowbox from pabouctsidis.alex is not active ;-(
I can download approx. 20-30MB and the connection is faild.
Konrad
2017-04-01 09:57 AM
https://drive.google.com/open?id=0B7OY5pub_GfIcGNtUW1XbjNYbnM
2017-04-24 06:57 AM
Hello Madam,
Now download problem with STM32cube F7_v170zip,After midway of download st server stop to send data,and download stop and it has no resume capability, So unable to download STM32CUBEF7_v170.Can you provide any that type of link ,which has resume capability of download.
2017-04-24 07:50 AM
Hi
Chopra.Haripankh
,Maybe a server is down for few minutes. Have you try the download through CubeMx or ST web page?
Here is the needed package of
https://drive.google.com/open?id=0B-KpPbIrv-E0Qi1XdmN1eERXUTQ
to find a way out of that situation.Thanks
Imen