2019-04-18 02:43 AM
Hi,
I have two Nucleo F411 board. When I connect the board to the computer with the USB ST_Link, one automatically reset and the other no. I don't want that the board automatically reset.
The HW configuration and program are exactly the same for the two board. The only change is that a board is a mb1136 c-04 (who reset) and the other is a mb1136 c-03 (who not reset).
I examine the two board but don't see any difference.
An idea to solve this problem ?
Thanks,
Lionel
2019-04-18 05:00 AM
ST-LINK firmwares are what?
2019-04-18 05:45 AM
Good question !
In fact, I don't know. I use AC6 in the two cases with same parameters.
But I can use ST-Link to upload the binary if that can solve my problem.
Is there a special options to check ?
Thanks,
Lionel
2019-04-19 08:31 AM
Well, I have updated to the latest ST-Link found but always the same problem : when I connect the board I have a reset of the board.
Another idea ?
Thanks,
Lionel
2023-06-30 07:02 AM
Dear Lionel,
your post is some years hold, but I was facing the same issue with a board buyed just some weeks ago.
I have a Nucleo F411RE board (MB1136 C-04), and use an external 5V power supply. Thus, my jumper 5 is on E5V.
Everything works well, but when I connect the USB cable to the PC, for communicating with the COM port, the board reboots.
I could solve this issue with:
- Downloading STSW-LINK007 ST-LINK upgrade, from the ST website
- Updating the ST-Link firmware to the latest version V2.J42.M27
Hope it helps,
Scaramo