cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-F401RE .bin file

emilywengster
Associate II

Hello, 

I'm Emily and I'm fairly new at using NUCLEO devices and ToF sensor. I would like to ask if a board NUCLEO-F401RE could only run one .bin file or could it run two .bin file? I'm currently trying out STSW-IMG035 but would like to have Gesture and Hand Posture running on one program instead of two. 

Also, I would also like two know if it is possible to have gesture and hand posture to run in one program as well. Any help is appreciated! 

Thank you!

 

Emily 

1 REPLY 1

Not exactly.

What you could more practically do is merge the functionality at a source code level and the allow it the select the demo to run.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..