2019-02-27 4:46 PM
2019-02-27 4:47 PM
Small correction.... the file is USBD_CONF.C (not USB_CONF.C as listed above)
2019-02-27 7:16 PM
for me prototype is at line 53 :
USBD_StatusTypeDef USBD_Get_USB_Status(HAL_StatusTypeDef hal_status);
but it is in the USER CODE section...
still i'm having issue with the usb virtual comport and the 1.24. The python script I was using with 1.23 can't connect. When using a more standard serial software it is ok (TeraTerm) but not with python and PYserial !
Note to myself, never upgrade cubeMX on an ongoing project !
2019-02-27 7:55 PM
My connection issue was soled with this post !
2019-12-22 4:23 PM
This applies both to usbh_conf.c and usbd_conf.c generated by STM32CubeMX v5.3.0
Adding the declaration in a user block (e.g. at line 53 in usbd_conf.c as suggested by @Community member solves the compilation error.
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
USBD_StatusTypeDef USBD_Get_USB_Status(HAL_StatusTypeDef hal_status);
/* USER CODE END PFP */
or for usbh_conf.c:
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
USBH_StatusTypeDef USBH_Get_USB_Status(HAL_StatusTypeDef hal_status);
/* USER CODE END PFP */
2019-12-22 5:28 PM
Update: this is still an issue with v5.4.0