2018-08-30 12:20 AM
im using STM32F030R8T6 (nucleo F030R8 board)
i tried to enable SPI2 peripheral clock, but i cant find any line in stm32f0xx_hal_rcc.h to enable spi2 clock,
but there is macro for SPI1
__HAL_RCC_SPI1_CLK_ENABLE()
only few marcos for RCC_APB1ENR present in stm32f0xx_hal_rcc.h is there any reason for this.
or iam i missed any configuration for stm32f030R8
firmware: STM32Cube_FW_F0_V1.9.0
Solved! Go to Solution.
2018-08-30 3:15 AM
Hi @mvigneshwaran27 ,
__HAL_RCC_SPI2_CLK_ENABLE is declared in stm32f0xx_hal_rcc_ex.h.
Tip: You can easily check it generating a project with STM32CubeMX where you enable SPI2 for your selected device (STM32F030R8Tx). __HAL_RCC_SPI2_CLK_ENABLE is called in HAL_SPI_MspInit (file: stm32f0xx_hal_msp.c).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-08-30 3:15 AM
Hi @mvigneshwaran27 ,
__HAL_RCC_SPI2_CLK_ENABLE is declared in stm32f0xx_hal_rcc_ex.h.
Tip: You can easily check it generating a project with STM32CubeMX where you enable SPI2 for your selected device (STM32F030R8Tx). __HAL_RCC_SPI2_CLK_ENABLE is called in HAL_SPI_MspInit (file: stm32f0xx_hal_msp.c).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.