cancel
Showing results for 
Search instead for 
Did you mean: 

No Example QSPI SDK for STM32F413H

avinpat_8
Associate III

Hi i am using Nucleo - F413ZH i need to work on the QSPI protocol i found this device supports QSPI but in the repository i doesn't find any example code for this one is this device supports QSPI? or is there any similar sdk so that we can import projects form other repository
I tried with the example code present in the STM32F413H-Discovery repository but i doesn't got output

avinpat_8_0-1742817721795.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @avinpat_8;

 

There are no QSPI examples for Nucleo - F413ZH.

Which memory is connected to the QUADSPI interface?

The QSPI examples are configured according to memory specifications.

The QSPI examples for STM32F413H-DISCOVERY board are tested with N25Q128A13EF840 micron, so you need to update the QSPI configuration in main.c and the command operation in main.h according to the memory you've used.

KDJEM1_0-1742818184560.png

I recommend you to look at the QSPI example and get inspired to create your own project.

Also, I advise you to look at AN4760 precisely 4. QUADSPI configuration section. This section describes all QUADSPI configuration steps required to perform either read, write or erase operations.

I hope this help you.

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
mÆŽALLEm
ST Employee

Hello,

You provided a contradictory information:


@avinpat_8 wrote:

 i found this device supports QSPI but in the repository i doesn't find any example code for this one is this device supports QSPI? 


Then you said:


@avinpat_8 wrote:

I tried with the example code present in the STM32F413H-Discovery repository but i doesn't got output


So the example is there. Why you said that the repository doesn't contain any QSPI example?

And this is the repository containing the QSPI examples: https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM32F413H-Discovery/Examples/QSPI

The examples don't contain any ioc file.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi can you check this repository where i have attached image

sorry for you confusion my point is QSPI sdk is present in the  STM32F413H-Discovery but my board is  Nucleo - F413ZH but in the repo of STM32F413ZH-Nucleo it is not present what my point is whether the device  Nucleo - F413ZH supports QSPI as i saw in STMcubeMX that peripheral was present

avinpat_8_0-1742818305211.png

 

 

avinpat_8_0-1742817871533.png

 

You are pointing to the NUCLEO board not to the Discovery board.

The NUCLEO board doesn't contain any external memory.

If you look for QSPI example running on STM32F413 device you need to check the example running on the Discovery board:

https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM32F413H-Discovery/Examples/QSPI

Hope that answers your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
KDJEM.1
ST Employee

Hello @avinpat_8;

 

There are no QSPI examples for Nucleo - F413ZH.

Which memory is connected to the QUADSPI interface?

The QSPI examples are configured according to memory specifications.

The QSPI examples for STM32F413H-DISCOVERY board are tested with N25Q128A13EF840 micron, so you need to update the QSPI configuration in main.c and the command operation in main.h according to the memory you've used.

KDJEM1_0-1742818184560.png

I recommend you to look at the QSPI example and get inspired to create your own project.

Also, I advise you to look at AN4760 precisely 4. QUADSPI configuration section. This section describes all QUADSPI configuration steps required to perform either read, write or erase operations.

I hope this help you.

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Kaouthar thanks for your reply i got your point

If your question has been answered please accept as solution the comment that answered your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.