2024-04-04 12:07 PM
Hello,
I'm trying to find out why nx_tcp_client_socket_connect is returning 0x38. This error code is not listed in documentation. Because of this, there is no ARP packet being sent.
static VOID nx_app_thread_entry (ULONG thread_input)
{
UINT status;
status = nx_tcp_socket_create(&NetXDuoEthIpInstance, &client_socket, "Client Socket",
NX_IP_NORMAL, NX_FRAGMENT_OKAY, NX_IP_TIME_TO_LIVE, 200,
NX_NULL, NX_NULL);
status = nx_tcp_client_socket_bind(&client_socket, 45450, NX_WAIT_FOREVER);
status = nx_tcp_client_socket_connect(&client_socket, IP_ADDRESS(192, 168, 15, 16), 45450, NX_IP_PERIODIC_RATE);
}