Need resources for STM32H563ZI nucleo board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-28 4:49 AM
I was recently working on STM32H563ZI nucleo board like connecting peripherals like LTE module, I2C sensors like MPU6050, LCD display, SPI modules like W25Q flash storage, USB and some analog module like potentiometer. As per normal coding of individual peripherals resources were available but for smooth integration of all the peripherals i was planning to use DMA for reducing the load for smooth operation. But i didn't get any clear documentation or resources of using GPDMA (present in STM32H563ZI) for I2C, SPI and UART. As i was planning to use FreeRTOS instead of Azure RTOS (ThreadX) because how to implement it as in this microcontroller there is USBX which works on ThreadX. I followed the resources on Youtube from official STMicroelecronics channel, followed the same but the code was not working as expected.
I was going through reference manual the peripheral was USB, that means it can be used without RTOS
I need help in resources for GPDMA for I2C,SPI and USART, USB with FreeRTOS or normal coding.
Solved! Go to Solution.
- Labels:
-
ST boards
-
STM32H5 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-28 5:15 AM - edited ‎2025-04-21 3:13 AM
Hello,
@Shubham08 wrote:
I was going through reference manual the peripheral was USB, that means it can be used without RTOS
Indeed. You can use USB without RTOS unless you are using a specific stack USBX for example.
The resources available are:
The datasheet of the product, the reference manual of the product and the STM32CubeH5 package examples.
@Shubham08 wrote:
I need help in resources for GPDMA for I2C,SPI and USART, USB with FreeRTOS or normal coding.
RTOS is not part of the product so you can't find any resources/information or coding in the reference manual nor in the datasheet.
For examples without RTOS, you can refer to the STM32CubeH5 package (especially on STM32H563ZI nucleo board) on this link.
For USB: https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/NUCLEO-H563ZI/Applications/USBX
For SPI, I2C, UART etc:
https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/NUCLEO-H563ZI/Examples
Hope that helps.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-28 5:01 AM
@Shubham08 wrote:i didn't get any clear documentation or resources of using GPDMA (present in STM32H563ZI) for I2C, SPI and UART. .
Those are internal features of the chip - they would not depend on the board.
So you need to look at the chip documentation:
https://www.st.com/en/microcontrollers-microprocessors/stm32h563zi.html#documentation
https://www.st.com/en/microcontrollers-microprocessors/stm32h563zi.html#tools-software
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-28 5:15 AM - edited ‎2025-04-21 3:13 AM
Hello,
@Shubham08 wrote:
I was going through reference manual the peripheral was USB, that means it can be used without RTOS
Indeed. You can use USB without RTOS unless you are using a specific stack USBX for example.
The resources available are:
The datasheet of the product, the reference manual of the product and the STM32CubeH5 package examples.
@Shubham08 wrote:
I need help in resources for GPDMA for I2C,SPI and USART, USB with FreeRTOS or normal coding.
RTOS is not part of the product so you can't find any resources/information or coding in the reference manual nor in the datasheet.
For examples without RTOS, you can refer to the STM32CubeH5 package (especially on STM32H563ZI nucleo board) on this link.
For USB: https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/NUCLEO-H563ZI/Applications/USBX
For SPI, I2C, UART etc:
https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/NUCLEO-H563ZI/Examples
Hope that helps.