cancel
Showing results for 
Search instead for 
Did you mean: 

Could I get SCHLIB files or pspice model for Nucle-F103 (MB1136)?

seho
Associate

Dear all,

I downloaded the schematic files for nucleo-64board(MB1136) from this page
(https://www.st.com/en/evaluation-tools/nucleo-f103rb.html#cad-resources)
and opened them in Altium.

However, when I tried to run a simulation, I encountered an error.

I believe I need an MB1136 SCHLIB file or SPICE library files
to properly simulate this board.

Could you please provide the SCHLIB file or a PSpice model for MB1136?

I apologize for any inconvenience, as I am new to Altium.

스크린샷 2025-04-09 133931.png

 Thank you

2 REPLIES 2
Laurent4
ST Employee

Hello Seho,

There are no models attached to the components in the Altium library in the shared schematics on ST.com

I'm not sure that this can address your point but :

To generate a schlib : on Altium Designer Menu:  Design -> Make Integrated Librairy ( or schematic Librairy) from the project open.

Best Regards .

 

Sco
ST Employee

If you consider it's an issue linked to the Lib, you can refer to MB1932:MB1932 - Resources - Search STMicrocontrollers. MB1932 is a board very similar to MB1136.