2024-04-06 3:33 AM - edited 2024-04-06 4:13 AM
当我想进入程序时,应用程序说“文件大小大于等于大小。”
我的文件是.hex
怎么解决这个问题呢?
stm32f103c8t6
18:55:25:与设备断开连接。
18:55:27 : ST-LINK SN
18:55:27 : V2J34S7
18:55:27 : 通过 SWD 连接。
18:55:27:SWD 频率 = 4.0 MHz。
18:55:27:连接模式:正常。
18:55:27:启用低功耗模式下的调试。
18:55:27:设备 ID:0x412
18:55:27:设备闪存大小:32KBytes
18:55:27:设备系列:STM32F10xx 低密度
18:55:44:文件大小大于闪存大小。
19:03:12 : [FreeJoy_v1_7_1b2.hex] 打开成功。
19:03:12 : [FreeJoy_v1_7_1b2.hex] 校验和 : 0x0096951C
19:03:20 : 文件大小大于闪存大小。
19:03:42 : 文件大小大于闪存大小。
19:05:40 : [FreeJoy_v1_7_1b2.bin] 打开成功。
19:05:40 : [FreeJoy_v1_7_1b2.bin] 校验和 : 0x0036395C
19:05:48 : 文件大小大于闪存大小。
19:09:47 : [FreeJoy_v1_01b4.hex] 打开成功。
19:09:47 : [FreeJoy_v1_01b4.hex] 校验和 : 0x00C6B4F8
19:09:56 : 文件大小大于闪存大小。
19:11:46:闪存已擦除。
19:12:01 : 文件大小大于闪存大小。
2024-04-16 7:55 AM - edited 2024-04-16 8:20 AM
Hello @ikun
Could you please provide additional details about the issue? What is the version of STM32Cube Programmer are you using? What is the size of your file?
Thanks
Omar
2024-04-16 9:14 AM
A 35KB binary is NOT going to fit on a part with 32KB of FLASH
>>How to solve this problem?
Perhaps program it on to a suitable part, or build in a way that's physically smaller?
https://github.com/FreeJoy-Team/FreeJoy/releases
https://github.com/FreeJoy-Team/FreeJoy/releases/download/v1.7.1b3/FreeJoy_v1_7_1b2.zip
2024-04-16 9:14 AM
When I want to enter the program, the application says "File size is greater than or equal to size."
My file is .hex
How to solve this problem?
stm32f103c8t6
18:55:25: Disconnected from device.
18:55:27 : ST-LINK SN
18:55:27 : V2J34S7
18:55:27 : Connect via SWD.
18:55:27: SWD frequency = 4.0 MHz.
18:55:27: Connection mode: Normal.
18:55:27: Enable debugging in low power mode.
18:55:27: Device ID: 0x412
18:55:27: Device flash size: 32KBytes
18:55:27: Device family: STM32F10xx low density
18:55:44: File size is larger than flash size.
19:03:12: [FreeJoy_v1_7_1b2.hex] opened successfully.
19:03:12 : [FreeJoy_v1_7_1b2.hex] Checksum: 0x0096951C
19:03:20 : File size is larger than flash memory size.
19:03:42 : File size is larger than flash size.
19:05:40: [FreeJoy_v1_7_1b2.bin] opened successfully.
19:05:40 : [FreeJoy_v1_7_1b2.bin] Checksum: 0x0036395C
19:05:48 : File size is larger than flash memory size.
19:09:47: [FreeJoy_v1_01b4.hex] opened successfully.
19:09:47 : [FreeJoy_v1_01b4.hex] Checksum: 0x00C6B4F8
19:09:56 : File size is larger than flash memory size.
19:11:46: Flash memory erased.
19:12:01 : File size is larger than flash size.