2024-04-23 1:59 AM
Hello,
I want to use the USBX MTP stack on a stm32u5 without threadx. The configuration in stm32CubeMx worked fine but when i run the programm, i get UX_FUNCTION_NOT_SUPPORTED from this location:
UINT _ux_device_class_pima_initialize(UX_SLAVE_CLASS_COMMAND *command)
{
#if defined(UX_DEVICE_STANDALONE)
UX_PARAMETER_NOT_USED(command);
return(UX_FUNCTION_NOT_SUPPORTED);
#else
UINT status;
UX_SLAVE_CLASS_PIMA *pima;
UX_SLAVE_CLASS_PIMA_PARAMETER *pima_parameter;
UX_SLAVE_CLASS *class_ptr;
Are there any other options to use the USBX MTP stack in standalone mode at the moment or are there any plans to support the standalone mode in the future?
Thanks in advance.
2024-05-02 8:37 AM
Hello Codgen,
Only RTOS mode is supported for USBX device pima class driver
Regards,
2024-05-02 8:44 AM
There are perhaps third-party commercial libraries or you could DIY