2021-10-03 5:04 PM
On a choisi X-CUBE-CLD-GEN pour connecter la carte avec mongodb via mosquitt
Après le flash de la carte par le fichier bin et la configuration du wifi par le terminal(tera
term), l’insertion de la certification du mongodb n’a pas marché.
2021-10-04 6:53 AM
Hi @NKhad.1 ,
In order to have more chance to get an answer, I am translating your post to English (commonly used language for our Community):
We chose X-CUBE-CLD-GEN to connect the board with mongodb via mosquitto. After downloading the bin file to the board and the configuration of the wifi by the terminal (teraterm), the inclusion of mongodb certification did not work.
Here I assume you are using B-L475E-IOT01 (based on your other question).
I also add relevant topic so that our experts can review this question.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-10-12 5:36 AM
Hello
What do you mean by "l’insertion de la certification du mongodb n’a pas marché" / "The inclusion of mongodb certification did not work" ? could you give more details ?