cancel
Showing results for 
Search instead for 
Did you mean: 

LWIP_RAND uses newlib rand() and fails

Gustavo_AR
Associate III

CubeMX generated project defines

 

#define LWIP_RAND() ((u32_t)rand())

 

which fails with the following call stack...

Gustavo_AR_1-1726157473699.png

and the following assert text

assertion "REENT malloc succeeded" failed: file "/build/gnu-tools-for-stm32_12.3.rel1.20240612-1315/src/newlib/newlib/libc/stdlib/rand.c", line 82

Line 82 of rand.c is:

 

_REENT_CHECK_RAND48(reent);

 

which in turn ends up calling a malloc... 

I've read that reentrancy in newlib could cause problems, but I thought it would be memory corruption.

Is there a solution for this?

Thanks in advance!

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @Gustavo_AR ,

Seems you have the same issue reported in these posts:

Hope the shared posts will help you, otherwise please share more details about the device, the tools version used and how to reproduce the issue.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

2 REPLIES 2
Imen.D
ST Employee

Hello @Gustavo_AR ,

Seems you have the same issue reported in these posts:

Hope the shared posts will help you, otherwise please share more details about the device, the tools version used and how to reproduce the issue.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Thanks @Imen.D I've fixed it by 

/* Defining malloc/free should overwrite the standard versions provided by the compiler. */ void *malloc(size_t size) { /* Call the FreeRTOS version of malloc. */ return pvPortMalloc(size); } void free(void *ptr) { /* Call the FreeRTOS version of free. */ vPortFree(ptr); }