2019-08-28 2:50 AM
Hi,
This is not an STM32 question, but more related to LWIP. Yet, maybe someone here will have an idea.
We use LWIP AS-IS from the example, and we test the Ethernet receive in high load with udp packets.
We see that when send from the tester device small packets ( less then 450 bytes), in high rate into the stm32, it gets into LWIP drop packet, because pcb is null. I thought that maybe there are not enough PCB, to I tried to increase UDP PCB packets, but I get the same results.
Thanks,
ranran
2019-08-28 4:18 AM
I would measure the system load, especially of the ethernet handling routines (interrupt or DMA) in relation to arriving metwork packages.
I suspect an overload.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.