2024-12-08 08:29 PM - last edited on 2024-12-09 12:22 AM by SofLit
Hi, I am using STM32F767ZI for ethernet communication. I update my CUBEIDE version from 1.16.1 to 1.17 latest version. After I update my ethernet program was show HardFault_Handler() during Execution. This was working fine in the previous version(1.16.1). In the new version(1.17) It hit the fault in mem_init() at mem.c (line no. 18).
void
mem_init(void)
{
struct mem *mem;
LWIP_ASSERT("Sanity check alignment",
(SIZEOF_STRUCT_MEM & (MEM_ALIGNMENT - 1)) == 0);
/* align the heap */
ram = (u8_t *)LWIP_MEM_ALIGN(LWIP_RAM_HEAP_POINTER);
/* initialize the start of the heap */
mem = (struct mem *)(void *)ram;
mem->next = MEM_SIZE_ALIGNED;
mem->prev = 0;
mem->used = 0;
/* initialize the end of the heap */
ram_end = ptr_to_mem(MEM_SIZE_ALIGNED);
ram_end->used = 1;
ram_end->next = MEM_SIZE_ALIGNED;
ram_end->prev = MEM_SIZE_ALIGNED; (In this line the hardware fault was occur)
MEM_SANITY();
/* initialize the lowest-free pointer to the start of the heap */
lfree = (struct mem *)(void *)ram;
MEM_STATS_AVAIL(avail, MEM_SIZE_ALIGNED);
if (sys_mutex_new(&mem_mutex) != ERR_OK) {
LWIP_ASSERT("failed to create mem_mutex", 0);
}
}
In LWIP setting, the HTTPD setting -> set the MEM_SIZE(Heap) = 10*1024.
I refer compare the previous version and latest version lwipopts.h file. The below line was added in the header file
/*----- Default Value for F7/H7 devices: 0x30044000 -----*/
#define LWIP_RAM_HEAP_POINTER 0x30044000 (updated version).
Let's give the guidance how to rectify this error during execution.
Thank you
Ramachandran.S
2024-12-09 01:53 AM
Hello @Ramachandran1992 ,
can you compare the two projects to see what the changes that are done in code beside the:
#define LWIP_RAM_HEAP_POINTER 0x30044000
and if you can check the default Ram pointer value before migration as well .
Regards
2024-12-09 03:21 AM - edited 2024-12-11 07:53 PM
Hi ST,
Yes, But didn't see no difference except the "LWIP_RAM_HEAP_POINTER". please notify anything was missing from my side. It hit the HardFault_Handler() in the mem_init() at mem.c file.
I insert the 2-version code the below code was version - 1.16.1
/* Define to prevent recursive inclusion --------------------------------------*/
#ifndef __LWIPOPTS__H__
#define __LWIPOPTS__H__
#include "main.h"
/*-----------------------------------------------------------------------------*/
/* Current version of LwIP supported by CubeMx: 2.1.2 -*/
/*-----------------------------------------------------------------------------*/
/* Within 'USER CODE' section, code will be kept by default at each generation */
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
#ifdef __cplusplus
extern "C" {
#endif
/* STM32CubeMX Specific Parameters (not defined in opt.h) ---------------------*/
/* Parameters set in STM32CubeMX LwIP Configuration GUI -*/
/*----- WITH_RTOS disabled (Since FREERTOS is not set) -----*/
#define WITH_RTOS 0
/*----- CHECKSUM_BY_HARDWARE enabled -----*/
#define CHECKSUM_BY_HARDWARE 1
/*-----------------------------------------------------------------------------*/
/* LwIP Stack Parameters (modified compared to initialization value in opt.h) -*/
/* Parameters set in STM32CubeMX LwIP Configuration GUI -*/
/*----- Value in opt.h for NO_SYS: 0 -----*/
#define NO_SYS 1
/*----- Value in opt.h for SYS_LIGHTWEIGHT_PROT: 1 -----*/
#define SYS_LIGHTWEIGHT_PROT 0
/*----- Value in opt.h for MEM_ALIGNMENT: 1 -----*/
#define MEM_ALIGNMENT 4
/*----- Default Value for MEM_SIZE: 1600 ---*/
#define MEM_SIZE 10*1024
/*----- Value in opt.h for LWIP_ETHERNET: LWIP_ARP || PPPOE_SUPPORT -*/
#define LWIP_ETHERNET 1
/*----- Value in opt.h for LWIP_DNS_SECURE: (LWIP_DNS_SECURE_RAND_XID | LWIP_DNS_SECURE_NO_MULTIPLE_OUTSTANDING | LWIP_DNS_SECURE_RAND_SRC_PORT) -*/
#define LWIP_DNS_SECURE 7
/*----- Value in opt.h for TCP_SND_QUEUELEN: (4*TCP_SND_BUF + (TCP_MSS - 1))/TCP_MSS -----*/
#define TCP_SND_QUEUELEN 9
/*----- Value in opt.h for TCP_SNDLOWAT: LWIP_MIN(LWIP_MAX(((TCP_SND_BUF)/2), (2 * TCP_MSS) + 1), (TCP_SND_BUF) - 1) -*/
#define TCP_SNDLOWAT 1071
/*----- Value in opt.h for TCP_SNDQUEUELOWAT: LWIP_MAX(TCP_SND_QUEUELEN)/2, 5) -*/
#define TCP_SNDQUEUELOWAT 5
/*----- Value in opt.h for TCP_WND_UPDATE_THRESHOLD: LWIP_MIN(TCP_WND/4, TCP_MSS*4) -----*/
#define TCP_WND_UPDATE_THRESHOLD 536
/*----- Value in opt.h for LWIP_NETIF_LINK_CALLBACK: 0 -----*/
#define LWIP_NETIF_LINK_CALLBACK 1
/*----- Value in opt.h for LWIP_NETCONN: 1 -----*/
#define LWIP_NETCONN 0
/*----- Value in opt.h for LWIP_SOCKET: 1 -----*/
#define LWIP_SOCKET 0
/*----- Value in opt.h for RECV_BUFSIZE_DEFAULT: INT_MAX -----*/
#define RECV_BUFSIZE_DEFAULT 2000000000
/*----- Default Value for LWIP_HTTPD: 0 ---*/
#define LWIP_HTTPD 1
/*----- Default Value for LWIP_HTTPD_CGI: 0 ---*/
#define LWIP_HTTPD_CGI 1
/*----- Default Value for LWIP_HTTPD_SSI: 0 ---*/
#define LWIP_HTTPD_SSI 1
/*----- Value in opt.h for LWIP_STATS: 1 -----*/
#define LWIP_STATS 0
/*----- Value in opt.h for CHECKSUM_GEN_IP: 1 -----*/
#define CHECKSUM_GEN_IP 0
/*----- Value in opt.h for CHECKSUM_GEN_UDP: 1 -----*/
#define CHECKSUM_GEN_UDP 0
/*----- Value in opt.h for CHECKSUM_GEN_TCP: 1 -----*/
#define CHECKSUM_GEN_TCP 0
/*----- Value in opt.h for CHECKSUM_GEN_ICMP: 1 -----*/
#define CHECKSUM_GEN_ICMP 0
/*----- Value in opt.h for CHECKSUM_GEN_ICMP6: 1 -----*/
#define CHECKSUM_GEN_ICMP6 0
/*----- Value in opt.h for CHECKSUM_CHECK_IP: 1 -----*/
#define CHECKSUM_CHECK_IP 0
/*----- Value in opt.h for CHECKSUM_CHECK_UDP: 1 -----*/
#define CHECKSUM_CHECK_UDP 0
/*----- Value in opt.h for CHECKSUM_CHECK_TCP: 1 -----*/
#define CHECKSUM_CHECK_TCP 0
/*----- Value in opt.h for CHECKSUM_CHECK_ICMP: 1 -----*/
#define CHECKSUM_CHECK_ICMP 0
/*----- Value in opt.h for CHECKSUM_CHECK_ICMP6: 1 -----*/
#define CHECKSUM_CHECK_ICMP6 0
/*-----------------------------------------------------------------------------*/
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
#ifdef __cplusplus
}
#endif
#endif /*__LWIPOPTS__H__ */
the below code was version - 1.17.0
/* Define to prevent recursive inclusion --------------------------------------*/
#ifndef __LWIPOPTS__H__
#define __LWIPOPTS__H__
#include "main.h"
/*-----------------------------------------------------------------------------*/
/* Current version of LwIP supported by CubeMx: 2.1.2 -*/
/*-----------------------------------------------------------------------------*/
/* Within 'USER CODE' section, code will be kept by default at each generation */
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
#ifdef __cplusplus
extern "C" {
#endif
/* STM32CubeMX Specific Parameters (not defined in opt.h) ---------------------*/
/* Parameters set in STM32CubeMX LwIP Configuration GUI -*/
/*----- WITH_RTOS disabled (Since FREERTOS is not set) -----*/
#define WITH_RTOS 0
/*----- CHECKSUM_BY_HARDWARE enabled -----*/
#define CHECKSUM_BY_HARDWARE 1
/*-----------------------------------------------------------------------------*/
/* LwIP Stack Parameters (modified compared to initialization value in opt.h) -*/
/* Parameters set in STM32CubeMX LwIP Configuration GUI -*/
/*----- Value in opt.h for NO_SYS: 0 -----*/
#define NO_SYS 1
/*----- Value in opt.h for SYS_LIGHTWEIGHT_PROT: 1 -----*/
#define SYS_LIGHTWEIGHT_PROT 0
/*----- Value in opt.h for MEM_ALIGNMENT: 1 -----*/
#define MEM_ALIGNMENT 4
/*----- Default Value for MEM_SIZE: 1600 ---*/
#define MEM_SIZE 10*1024
/*----- Default Value for F7/H7 devices: 0x30044000 -----*/
#define LWIP_RAM_HEAP_POINTER 0x30044000
/*----- Value in opt.h for LWIP_ETHERNET: LWIP_ARP || PPPOE_SUPPORT -*/
#define LWIP_ETHERNET 1
/*----- Value in opt.h for LWIP_DNS_SECURE: (LWIP_DNS_SECURE_RAND_XID | LWIP_DNS_SECURE_NO_MULTIPLE_OUTSTANDING | LWIP_DNS_SECURE_RAND_SRC_PORT) -*/
#define LWIP_DNS_SECURE 7
/*----- Value in opt.h for TCP_SND_QUEUELEN: (4*TCP_SND_BUF + (TCP_MSS - 1))/TCP_MSS -----*/
#define TCP_SND_QUEUELEN 9
/*----- Value in opt.h for TCP_SNDLOWAT: LWIP_MIN(LWIP_MAX(((TCP_SND_BUF)/2), (2 * TCP_MSS) + 1), (TCP_SND_BUF) - 1) -*/
#define TCP_SNDLOWAT 1071
/*----- Value in opt.h for TCP_SNDQUEUELOWAT: LWIP_MAX(TCP_SND_QUEUELEN)/2, 5) -*/
#define TCP_SNDQUEUELOWAT 5
/*----- Value in opt.h for TCP_WND_UPDATE_THRESHOLD: LWIP_MIN(TCP_WND/4, TCP_MSS*4) -----*/
#define TCP_WND_UPDATE_THRESHOLD 536
/*----- Value in opt.h for LWIP_NETIF_LINK_CALLBACK: 0 -----*/
#define LWIP_NETIF_LINK_CALLBACK 1
/*----- Value in opt.h for LWIP_NETCONN: 1 -----*/
#define LWIP_NETCONN 0
/*----- Value in opt.h for LWIP_SOCKET: 1 -----*/
#define LWIP_SOCKET 0
/*----- Value in opt.h for RECV_BUFSIZE_DEFAULT: INT_MAX -----*/
#define RECV_BUFSIZE_DEFAULT 2000000000
/*----- Default Value for LWIP_HTTPD: 0 ---*/
#define LWIP_HTTPD 1
/*----- Default Value for LWIP_HTTPD_CGI: 0 ---*/
#define LWIP_HTTPD_CGI 1
/*----- Default Value for LWIP_HTTPD_SSI: 0 ---*/
#define LWIP_HTTPD_SSI 1
/*----- Value in opt.h for LWIP_STATS: 1 -----*/
#define LWIP_STATS 0
/*----- Value in opt.h for CHECKSUM_GEN_IP: 1 -----*/
#define CHECKSUM_GEN_IP 0
/*----- Value in opt.h for CHECKSUM_GEN_UDP: 1 -----*/
#define CHECKSUM_GEN_UDP 0
/*----- Value in opt.h for CHECKSUM_GEN_TCP: 1 -----*/
#define CHECKSUM_GEN_TCP 0
/*----- Value in opt.h for CHECKSUM_GEN_ICMP: 1 -----*/
#define CHECKSUM_GEN_ICMP 0
/*----- Value in opt.h for CHECKSUM_GEN_ICMP6: 1 -----*/
#define CHECKSUM_GEN_ICMP6 0
/*----- Value in opt.h for CHECKSUM_CHECK_IP: 1 -----*/
#define CHECKSUM_CHECK_IP 0
/*----- Value in opt.h for CHECKSUM_CHECK_UDP: 1 -----*/
#define CHECKSUM_CHECK_UDP 0
/*----- Value in opt.h for CHECKSUM_CHECK_TCP: 1 -----*/
#define CHECKSUM_CHECK_TCP 0
/*----- Value in opt.h for CHECKSUM_CHECK_ICMP: 1 -----*/
#define CHECKSUM_CHECK_ICMP 0
/*----- Value in opt.h for CHECKSUM_CHECK_ICMP6: 1 -----*/
#define CHECKSUM_CHECK_ICMP6 0
/*-----------------------------------------------------------------------------*/
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
#ifdef __cplusplus
}
#endif
#endif /*__LWIPOPTS__H__ */
I compare all the programs with previous version (1.16.1) and new version (1.17.0) there was no changes in the except this HardFault_Handler(). This fault was done during program was after hit the run, this fault occurred during the execution of MX_LWIP_Init() at mem_init() at mem.c. how to rectify this fault?