Hello, The STM32CubeH5 firmware package currently does not support the OEMiROT example on the STM32H523 device.The OEMiROT example for the STM32H533 cannot be compiled on the STM32H523 device because the STM32H523 lacks support for the CRYP and PKA p...
Hello @priyanka.yadav ,Could you please check your bootloader version. if it is V13.0, according to AN2506 table 164, the USART3 is not working.With regards
Hello @RS62,I tested the Open Bootloader application from my side using USART1, and it works well, could you please check:1/ USART1 pins are well connected:TX board pin PA9 connected to RX hostRX board pin PA10 connected to TX host2/ Bootloader activ...
Hello @PM.5 I have reported this request internally. Internal ticket number: 189199 (This is an internal tracking number and is not accessible or usable by customers).Thank you for your contribution