2018-01-26 7:55 AM
Hi there,
we are currently developing the firmware for our custom board with an STM32F746 MCU in LQFP-100 package. Our current version is working well and now we want to be able to download updates via USB DFU. I read many posts and the related documents from ST, so there might be some ways to realize this. Unfortunately, in either way we get stuck on choosing the right addresses or verifying code with DfuSe. My favorite way is the following in which we jump to the internal bootloader:
&sharpdefine SYS_MEM_ADD 0x1FF00000
//Disables the RCC (reset setting)HAL_RCC_DeInit();SysTick->CTRL = 0;SysTick->LOAD = 0;SysTick->VAL = 0;
// disables every IRQ
__disable_irq();// remap system memory to 0x0000 0000
SYSCFG->MEMRMP = 0x01;JumpToApplication = (void (*)(void)) (*((uint32_t *)(SYS_MEM_ADD + 4)));
__set_MSP(*(__IO uint32_t*) SYS_MEM_ADD);JumpToApplication();
while(1);
The problem is that this way is just working in debug mode (toolchain SW4STM32 with Segger J-link). So my breakpoint is at JumpToApplication() and when I go one step further the device appears in DfuSe with the correct memory mapping (DFU update possible). In normal run mode the application is running and while switching to DFU/Bootloader mode the MCU just resets. I tried some different addresses but nothing would work. Maybe there is another way or something wrong in the IDE settings?
I appreciate every help. Thanks in advance!
Regards,
Kevin Lehzen
#stm32f7Solved! Go to Solution.
2018-04-22 11:57 AM
,
,
Kevin, Clyde,
In the spirit of paying it forward, here is a working version using Atollic format for the F765.
,
Reset_Handler:,
ldr r0, =0x2004FFF0,
ldr r1, =0xDEADBEEF,
ldr r2, [r0, ♯ 0],
str r0, [r0, ♯ 0],
cmp r2, r1,
beq Reboot_Loaderldr sp, =_estack /* set stack pointer */
,
/* Copy the data segment initializers from flash to SRAM */,
movs r1, ♯ 0,
b LoopCopyDataInitldr r0, =SystemInit
,
blx r0,
bl mainReboot_Loader:
,
ldr r0, =0x1FF00000,
ldr sp, [r0, ♯ 0],
ldr r0, [r0, ♯ 4],
bx r0LoopForever:
,
b LoopForeverCopyDataInit:
,
ldr r3, =_sidata,
ldr r3, [r3, r1],
str r3, [r0, r1],
adds r1, r1, ♯ 4,
,
LoopCopyDataInit:,
ldr r0, =_sdata,
ldr r3, =_edata,
adds r2, r0, r1,
cmp r2, r3,
bcc CopyDataInit,
ldr r2, =_sbss,
b LoopFillZerobss,
/* Zero fill the bss segment. */,
FillZerobss:,
movs r3, ♯ 0,
str r3, [r2], ♯ 4,
,
LoopFillZerobss:,
ldr r3, = _ebss,
cmp r2, r3,
bcc FillZerobss/* Call the clock system initialization function.*/
,
bl SystemInit,
/* Call static constructors */,
bl __libc_init_array,
/* Call the application's entry point.*/,
bl main,
bx lr,
.size Reset_Handler, .-Reset_HandlerThanks Clive!
2018-09-11 8:22 AM
Well the forum transition seems to have made a dog's breakfast of the original post, and is apparently too large and malformed to bring up the editor window.
This brought up 'STM32 BOOTLOADER' on the STM32F746G-DISCO for me
//***************************************************************************
void BootDFU(void)
{
printf("Entering Boot Loader..\r\n");
SCB_DisableDCache();
*((unsigned long *)0x2004FFF0) = 0xDEADBEEF; // 320KB STM32F7xx
__DSB();
NVIC_SystemReset();
}
//***************************************************************************
; Reset handler
Reset_Handler PROC
EXPORT Reset_Handler [WEAK]
IMPORT SystemInit
IMPORT __main
LDR R0, =0x2004FFF0 ; Address for RAM signature
LDR R1, =0xDEADBEEF
LDR R2, [R0, #0]
STR R0, [R0, #0] ; Invalidate
CMP R2, R1
BEQ Reboot_Loader
LDR R0, =SystemInit
BLX R0
LDR R0, =__main
BX R0
ENDP
Reboot_Loader PROC
EXPORT Reboot_Loader ; STM32F7xx
LDR R1, =0xE000ED00 ; SCB
LDR R0, =0x1FF00000 ; ROM BASE
STR R0, [R1, #8] ; VTOR
LDR SP, [R0, #0] ; SP @ +0
LDR R0, [R0, #4] ; PC @ +4
BX R0
ENDP ; sourcer32@gmail.com
//***************************************************************************
2018-09-11 8:44 AM
2018-09-26 6:27 AM
@Community member hi Clive,
Can you help me with the JumpToApplication() in STM32F767 in IAR? After programming the flash inside my program, I only call this function (I don't know where to config the regs etc.)
#define FIRMWARE_ADDR 0x080C0000
JumpToApplication = (void (*)(void)) (*((uint32_t *)(FIRMWARE_ADDR+ 4)));
__set_MSP(*(__IO uint32_t*) FIRMWARE_ADDR);
JumpToApplication();
Thank you very much,
Duy
2018-09-26 8:02 AM
Why couldn't this have been a new thread, it's off-topic here?
Ok, that is at the base of FLASH, wouldn't the processor automatically be calling that?
Normally you put the loader at 0x08000000 and the app deeper in, like 0x08008000
The registers are described in the Reference Manual.
What's not working with the code here? Have you stepped into it? Are you building the App for that address base, or somewhere else?
2018-09-26 8:47 AM
Oh sorry, my bad, the address I jumped to was 0x080C0000
I disabled the interrupt but something keep the code stuck in the RCC init function.
2018-09-26 8:50 AM
Interrupts must be enabled on the app side if you do that. Also make sure that SCB->VTOR in SystemInit() within the App reflects the new base address for the image.
Have a fault handler that outputs useful data for diagnostics.
2018-09-26 9:42 AM
It runs now, thank you Clive