cancel
Showing results for 
Search instead for 
Did you mean: 

Issue Generating SBUS Signal on STM32F303ZET6 (Timing/Framing Problem)

Safana_Ismail
Associate
/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2025 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include <stdio.h> #include <string.h> #include "time.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ //#define SBUS_FRAME_PERIOD_MS 3.3f /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ TIM_HandleTypeDef htim2; UART_HandleTypeDef huart2; /* USER CODE BEGIN PV */ uint16_t channels[16]= { 1000, 900, 1200, 900, 1500, 1500, 1500, 1500, 1500, 1500, 1500, 1500, 1500, 1500, 1500, 1500 }; //uint8_t sbus_test[25] = { // 0x0F, // SBUS header // 0x00, 0x04, 0x10, 0x20, // Ch0–1 data bits // 0x40, 0x80, 0x00, 0x00, // Ch2–5 // 0x00, 0x00, 0x00, 0x00, // Ch6–9 // 0x00, 0x00, 0x00, 0x00, // Ch10–13 // 0x00, 0x00, 0x00, 0x00, // Ch14–15 // 0x00, // Flags // 0x00 // End byte //}; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_USART2_UART_Init(void); static void MX_TIM2_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ void SBUS_GenerateFrame(uint16_t channels[16], uint8_t sbus_data[25]) { memset(sbus_data, 0, 25); sbus_data[0] = 0x0F; uint32_t ch[16]; for (int i = 0; i < 16; i++) { // ch[i] = channels[i] & 0x07FF; // 11-bit channel data ch[i]=channels[i]; } // sbus_data[0] = 0x0F; sbus_data[1] = (uint8_t)(ch[0] & 0xFF); sbus_data[2] = (uint8_t)((ch[0] >> | (ch[1] << 3)); sbus_data[3] = (uint8_t)((ch[1] >> 5) | (ch[2] << 6)); sbus_data[4] = (uint8_t)(ch[2] >> 2); sbus_data[5] = (uint8_t)((ch[2] >> 10) | (ch[3] << 1)); sbus_data[6] = (uint8_t)((ch[3] >> 7) | (ch[4] << 4)); sbus_data[7] = (uint8_t)((ch[4] >> 4) | (ch[5] << 7)); sbus_data[8] = (uint8_t)(ch[5] >> 1); sbus_data[9] = (uint8_t)((ch[5] >> 9) | (ch[6] << 2)); sbus_data[10] = (uint8_t)((ch[6] >> 6) | (ch[7] << 5)); sbus_data[11] = (uint8_t)(ch[7] >> 3); sbus_data[12] = (uint8_t)(ch[8] & 0xFF); sbus_data[13] = (uint8_t)((ch[8] >> | (ch[9] << 3)); sbus_data[14] = (uint8_t)((ch[9] >> 5) | (ch[10] << 6)); sbus_data[15] = (uint8_t)(ch[10] >> 2); sbus_data[16] = (uint8_t)((ch[10] >> 10) | (ch[11] << 1)); sbus_data[17] = (uint8_t)((ch[11] >> 7) | (ch[12] << 4)); sbus_data[18] = (uint8_t)((ch[12] >> 4) | (ch[13] << 7)); sbus_data[19] = (uint8_t)(ch[13] >> 1); sbus_data[20] = (uint8_t)((ch[13] >> 9) | (ch[14] << 2)); sbus_data[21] = (uint8_t)((ch[14] >> 6) | (ch[15] << 5)); sbus_data[22] = (uint8_t)(ch[15] >> 3); sbus_data[23] = 0x00; // flags sbus_data[24] = 0x00; // end byte // printf("sbus_data= "); // for(int i=0;i<16;i++) // printf(" %d ",sbus_data[i] ); // printf("\r\n"); } void SBUS_Transmit(UART_HandleTypeDef *huart, uint16_t channels[16]) { uint8_t sbus_data[25]; SBUS_GenerateFrame(channels, sbus_data); HAL_UART_Transmit(huart, sbus_data, 25, HAL_MAX_DELAY); } //void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) //{ // if (htim->Instance == TIM2) // { // SBUS_Transmit(&huart2, channels); // Call your SBUS send function here //// HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_0); //// HAL_UART_Transmit(&huart2, sbus_test, 25, 3.3); // } //} /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_USART2_UART_Init(); MX_TIM2_Init(); /* USER CODE BEGIN 2 */ // HAL_TIM_Base_Start_IT(&htim2); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { // // SBUS_Transmit(&huart2, channels); // HAL_Delay(10); HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_0); /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_PeriphCLKInitTypeDef PeriphClkInit = {0}; /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9; RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV1; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) { Error_Handler(); } PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_TIM2; PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1; PeriphClkInit.Tim2ClockSelection = RCC_TIM2CLK_HCLK; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK) { Error_Handler(); } } /** * @brief TIM2 Initialization Function * None * @retval None */ static void MX_TIM2_Init(void) { /* USER CODE BEGIN TIM2_Init 0 */ /* USER CODE END TIM2_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0}; /* USER CODE BEGIN TIM2_Init 1 */ /* USER CODE END TIM2_Init 1 */ htim2.Instance = TIM2; htim2.Init.Prescaler = 71; htim2.Init.CounterMode = TIM_COUNTERMODE_UP; htim2.Init.Period = 3299; htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim2) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } if (HAL_TIM_OC_Init(&htim2) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK) { Error_Handler(); } sConfigOC.OCMode = TIM_OCMODE_TIMING; sConfigOC.Pulse = 0; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM2_Init 2 */ /* USER CODE END TIM2_Init 2 */ HAL_TIM_MspPostInit(&htim2); } /** * @brief USART2 Initialization Function * None * @retval None */ static void MX_USART2_UART_Init(void) { /* USER CODE BEGIN USART2_Init 0 */ /* USER CODE END USART2_Init 0 */ /* USER CODE BEGIN USART2_Init 1 */ /* USER CODE END USART2_Init 1 */ huart2.Instance = USART2; huart2.Init.BaudRate = 100000; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_2; huart2.Init.Parity = UART_PARITY_EVEN; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_TXINVERT_INIT; huart2.AdvancedInit.TxPinLevelInvert = UART_ADVFEATURE_TXINV_ENABLE; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART2_Init 2 */ /* USER CODE END USART2_Init 2 */ } /** * @brief GPIO Initialization Function * None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET); /*Configure GPIO pin : PB0 */ GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * file: pointer to the source file name * line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more

Hello ST Community,

I'm facing an issue Generating and transmitting SBUS signals on a (STM32F303ZET6) NUCLEO F303ZE board.

  1. [Part Number]

STM32F303ZET6 (LQFP144, ARM Cortex-M4)

  1. [Environment]
  • Toolchain: STM32CubeIDE v[YourVersion]

  • HAL or LL Drivers: [HAL/LL version]

  • Debug Interface: ST-Link V2

  • Board:  Nucleo-F303ZE 
  • UART configured at 100000 baud, 8E2 Inverted
  1. [Details – Problem Description]
    I’m trying to generate an SBUS signal on a UART configured for 100000 baud, 8E2 using STM32F303ZET6. The signal is meant to replicate a Futaba-compatible SBUS stream with 25-byte frames at ~7ms intervals.

However:

  • The output frame timing or logic levels are inconsistent.

  • Some receivers fail to detect valid SBUS frames.

  • (Include screenshots from logic analyzer/scope if available)

  1. [Expected Behavior]
  • Consistent, valid SBUS frames every 7ms

  • UART configured to send SBUS frames that match the Futaba protocol:

    • Start byte: 0x0F

    • 22 bytes of data (16 channels packed)

    • 1 flag byte

    • End byte: 0x00

  1. [How to Reproduce]
  1. Configure UARTx on STM32F303ZET6 to 100000 baud, Even parity, 2 stop bits

  2. Transmit hardcoded SBUS frame buffer (25 bytes)

  3. Observe output on logic analyzer or oscilloscope

  4. Attempt to read signal on SBUS-compatible receiver or decoder

  1. [Occurrence]

 


Systematic: Happens every time I transmit SBUS

One or two time the sbus was detected when i transmitted only 16 bytes via uart with using command

memset(sbus_data, 0, 16);

 HAL_UART_Transmit(huart, sbus_data, 16, HAL_MAX_DELAY);

  1. [Sanity Checks Performed]
  • Verified baud, parity, and stop bits

  • Manually calculated timing of each byte

  • Compared with SBUS specification and working SBUS signal from known-good transmitter

  • Attempted both HAL and LL UART implementations

  • Searched STM32 forums and GitHub for existing SBUS implementations



0 REPLIES 0