2023-03-23 5:58 AM
Hey all,
I would like to make a HID device which would have output options configured by computer, I thought I would use same USB to feed the config to STM, But I cant seem to find a clear answer if it is even possible to send data to USB HID, like you do with CDC.
If anyone has clear answer or can point me towards documentation/example for that, I'd appreciate it.
Solved! Go to Solution.
2023-03-24 1:04 AM
Here seems to be the easiest option composite device - first class will be your HID keyboard, second class would serve for switching keyboard modes from host device, could be custom HID as well.
2023-03-23 6:41 AM
Hi,
you may check following guidance
https://www.youtube.com/watch?v=3JGRt3BFYrM&list=PLnMKNibPkDnFFRBVD206EfnnHhQZI4Hxa&index=16
But honestly right now I don't see any significant advantage compared to CDC. Could you please share why you want to prefer HID over CDC?
2023-03-23 6:53 AM
HID devices are easier to recognize (vs. multiple COM ports) by software.
The modern Windows has .net API to help with this.
2023-03-23 7:24 AM
Hey Lubos, Thanks for your answer, I want to use HID because I want my device to act as a keyboard when connected to pc. As far as I know, HID is the only way to do it (?).
2023-03-24 1:04 AM
Here seems to be the easiest option composite device - first class will be your HID keyboard, second class would serve for switching keyboard modes from host device, could be custom HID as well.