cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to have a custom bootloader in any sector?

Kenji1
Senior

Hi Team

I'm working on custom bootloader.

And I want to know if it possible to locate a custom bootloader in any sector.

Is it okay if the boot loader is not in the first address of FLASH 0x08000000?

[My Conditions]

IDE: STM32CubeIDE

MCU: STM32F405RG

1 ACCEPTED SOLUTION

Accepted Solutions

The F4 assumes bootable code/vector table is located at the base of FLASH (or ROM/RAM depending on mapping via BOOTx pins)

The H7 has some more options, but your bootloader needs to reside in the first 16KB FLASH block. You can put your App code anywhere you like deeper into the FLASH memory.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

4 REPLIES 4

Check if there is a "boot address" in option bytes (probably does not exists on this MCU).

Put boot loader at 0x08000000, check some condition during ~100ms after boot and proceed to main application in sector 1. Sector 0 (bootloader) may be write protected to keep device from being bricked during firmware update.

MM..1
Chief III

Exactly normal no, but you can use bigger system technology bootloader level 0 , in addr from mcu start this jump to any sector bootloadeer level 1 and here you start to app....

The F4 assumes bootable code/vector table is located at the base of FLASH (or ROM/RAM depending on mapping via BOOTx pins)

The H7 has some more options, but your bootloader needs to reside in the first 16KB FLASH block. You can put your App code anywhere you like deeper into the FLASH memory.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Kenji1
Senior

Hi, everyone!

Thank you for the reply.

I tested some codes, and F4 needs to locate the boot code on base address of FLASH.

Thanks.