2023-06-16 11:14 PM
Hello
I am newbie to embedded word. I am trying to learn interrupt for GPIO on NUCLEO-F091RC. I set the User Button as interrupt and LED should toggle as button is pressed. I copied the callback function ( HAL_GPIO_EXTI_Callback) in main.c . Under callback function, I called HAL_GPIO_Toggle . The code is working as expected.
But now I want LED to Blink as interrupt from button is generated. I wrote the below code. But as soon code comes to HAL_Delay function , it hangs. I tried to check in debug mode also. As I come to HAL_Delay function- StepInto , StepOver button fades out and code hangs there.
************************************************
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
while(1)
{
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
HAL_Delay(1000);
}
}
2023-06-17 12:39 AM
Cube/HAL is open source so you can check what's going on by reading those sources.
Delay in Cube/HAL generally depends on interrupt, usually SysTick, so if you don't assign proper priorities to that and your interrrupts, while in your interrupt, the delay-related interrupt can't fire and advance its counter.
JW
2023-06-17 9:12 AM
ISR (interrupt service routines) should be exited as quick as possible and kept as short as possible, delays in and ISR are a bad idea because you block what has a lower interrupt priority in the mcu. On top of that as explained by @waclawek.jan above, if your hardware ISR has a higher priority than the SysTick ISR that is the driver of the time count in HAL_Delay(), HAL_Delay cannot work anymore and your HAL_Delay waits forever for ticks that do not come any more.
The alternative is to set a flag and use the main() loop to organize the blinking:
/* USER CODE BEGIN PV */
#define TRUE 1 // JOHI
#define FALSE 0 // JOHI
volatile uint8_t buttonPressedFlag=FALSE; // JOHI
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
/* USER CODE BEGIN PFP */
// JOHI:
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
/* Prevent unused argument(s) compilation warning */
if (GPIO_Pin==BUTTON_Pin)
buttonPressedFlag=TRUE;
}
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
// JOHI:
if (buttonPressedFlag==TRUE)
{
HAL_GPIO_TogglePin(LED_GPIO_Port,LED_Pin);
HAL_Delay(1000);
HAL_GPIO_TogglePin(LED_GPIO_Port,LED_Pin);
HAL_Delay(1000);
buttonPressedFlag=FALSE;
}
HAL_Delay(10);
}
/* USER CODE END 3 */
}