cancel
Showing results for 
Search instead for 
Did you mean: 

Internal temperature Sensor STM32H743ZIT6

SITARAM
Associate III

I am using internal Temperature Sensor stm32h743zit6 , i notice  that when i connect power some time after that  it stable temperature approximately 46 degree or 47   degree, after i start streaming it came temperature also stable on this 46 degree or 47   degree temperature ,so when i work or not work continues but i   give continues power always stable it give stable temperature after some time  46 degree or 47 ..but when i heat external 50 degree Celsius then it came internal Temperature 51 degree Celsius , again i heat external 60 degree Celsius then it came internal Temperature 58 degree Celsius so can you tell me behavior of internal Temperature Sensor stm32h743zit6!!!!!!!!

so it is true that if i work or not but it give continues power supply  than  after some time it will always stable 46 or 47 degree Celsius and if i do external heat it will increase according to external heat provide if it true than explain it if false than why it came ????????????????????????

but i doing some internal work just like streaming  than it is possible to increase temperature from the stable temperature ,it is possible to increase  or it give stable temperature 46 0r 47 degree ????????????? 

 

 

 

2 REPLIES 2
Andrew Neil
Evangelist III

This sounds like entirely expected behaviour.

The operation of the chip generates heat internally.

The so-called thermal resistance of the package means that the internal temperature will be higher than the external temperature.

When you artificially raise the external temperature, the process is reversed - heat flows into the package, and the thermal resistance means that the internal temperature is lower than the external.

Take a look a this article - Basics of Thermal Resistance and Heat Dissipation:

https://fscdn.rohm.com/en/products/databook/applinote/common/basics_of_thermal_resistance_and_heat_dissipation_an-e.pdf

 

Addendum:

AndrewNeil_2-1726577499188.png

https://www.st.com/resource/en/datasheet/stm32h743zi.pdf#page=345 

 

See also AN5036, Guidelines for thermal management on STM32 applications:

https://www.st.com/resource/en/application_note/an5036-guidelines-for-thermal-management-on-stm32-applications-stmicroelectronics.pdf 

 

Andrew Neil
Evangelist III

@SITARAM wrote:

it is possible to increase temperature from the stable temperature ,it is possible to increase  or it give stable temperature 46 0r 47 degree ?


Power Dissipation is closely related to current consumption:

AndrewNeil_1-1726577261103.png

So take a look at those Tables 30 - 38 (on the following pages of the datasheet) to see what's going to make the most significant difference to current consumption ...

https://www.st.com/resource/en/datasheet/stm32h743zi.pdf#page=110