cancel
Showing results for 
Search instead for 
Did you mean: 

Reset & Wi-Fi SoftAP Initialization Failures with STM32H723ZGT6 + ST67W611M1

Grace_04
Associate II

Hi ST community,
I am using STM32H723ZGT6 as the host MCU with the ST67W611M1 Wi-Fi + BLE module.
Software details:
Firmware flashed on ST67: T01 binary
STM32 firmware package: X-CUBE-ST67W61(1.1.0)
Application selected: BLE P2P
Enabled parameters:
Wi-Fi SAP: Yes
Wi-Fi STA: Yes
BLE: Yes
NET: Yes
DHCP: STA+SAP
Issues observed:
Intermittent failure after reset in debug mode
When I reset the board while running in debug mode, the system sometimes does not work correctly(w6x init failed or other intiliazation failed in mainapp.c). The behavior is inconsistent—occasionally it works, but often it fails after reset.
Wi-Fi SoftAP start failure
The following API fails:
ret = W6X_WiFi_StartAp(&ap_config);
While debugging, the failure occurs due to a timeout in the following function:
/* Initialize the dual interface mode */
ret = TranslateErrorStatus(W61_WiFi_SetDualMode(p_DrvObj));
SPI clock configuration doubt
Could you please confirm the recommended SPI clock frequency for STM32H723ZGT6 when interfacing with ST67W611M1?
Should it be 40 MHz, or is a lower frequency required for stable operation?
DMA and linker script configuration
Is it necessary to modify the linker script for STM32H723ZGT6 to support DMA buffers (for example, placing buffers in non-cacheable memory)?
Could incorrect cache/DMA memory configuration cause the above intermittent failures or timeouts?
I have configured the board according to the document “How to use the X-CUBE-ST67W61 software package”, but the issue still persists.
Please let me know if any additional configuration, firmware version, or hardware constraint needs to be considered.
i attached the corresponding .ioc and mainapp.c files.
Thank you for your support.

0 REPLIES 0