2022-01-02 5:11 AM
Hi,
I've CubeIDE project for LAN9303 2 port ethernet driver. Followed the ST LWIP article and got the ping on the switch IC to PC.
I have a problem with getting registers of lan9303. I guess the LAN8742 driver is doing minimal settings on the ic but when I want to take the ic system and status registers, returns 0xFFFF. I am using lan8742 read-write functions in its driver. IO.ReadReg(pObj->DevAddr, ***, ®value)
Is there any specific read function to handle ic smi system registers? I just want to read 13.2.2.4 LED Configuration Register (LED_CFG).
Not: I2C is connected but I didn't use it, I guess my current configuration strap doesn't need to use it.
Regards,
Umit
2023-02-28 12:23 AM
Hi!
Sorry for digging up the post, but I'm trying to get a LAN9303 to work with an STM32F753 myself.
Surprisingly, I don't see in the Cube how to activate the LWIP (it's greyed out...).
How did you manage to activate it?
To sum up my project, I'm looking to do something simple:
My electronic card is connected to a PC via a Switch (3 sockets on the Switch - 2 to the card (lan9303) - 1 to the PC).
From my electronic card, I want to send two Ping commands to the PC (one from each of the LAN9303 ports).
Would you have an example that I can figure out how to achieve this?
2023-03-18 2:03 PM
Hello, we are using STM32H745 with LAN9303. We have 3 ports have you managed to activate it? If so can share the details of it.