2019-08-20 1:15 AM
Hello'
I'm looking for compact software package that supports UDP/DMA/ETH read/receive data according to the following rules:
Thanks in advance for yours assistance,
AlexE
2019-08-20 5:21 AM
Plenty of examples with and without RTOS:
\STM32Cube_FW_F7_V1.15.0\Projects\STM32756G_EVAL\Applications\LwIP
\STM32Cube_FW_F7_V1.15.0\Projects\STM32F769I_EVAL\Applications\LwIP
HAL and "compact" are two opposite terms.
P.S. Reliable, performant and compact lwIP examples fulfill only the 3rd point - they are invisible. :)
2019-09-11 1:31 AM
Hello Piranha,
Thank you very much for your answer,
Now I back to the problem...
We changed our platform from F7 to STM32H743ZI and I made new UdpEchoClient application using source STM32H743ZI _EVAL\Applications\LwIP (in other word UdpEchoClient for Nucleo144) without RTOS!
Unfortunately , it doesn't work ...
Maybe you know about any working UdpEchoClient /Server without RTOS (location, download ?
PS: When I try to built trivial Ethernet sample using MX (STM32CubeIDE/MX) it says me that LwIP cannot be attached if RTOS is not enabled - ?
Thanks Alexp
2019-09-11 1:32 AM
Hello Piranha,
Thank you very much for your answer,
Now I back to the problem...
We changed our platform from F7 to STM32H743ZI and I made new UdpEchoClient application using source STM32H743ZI _EVAL\Applications\LwIP (in other word UdpEchoClient for Nucleo144) without RTOS!
Unfortunately , it doesn't work ...
Maybe you know about any working UdpEchoClient /Server without RTOS (location, download ?
PS: When I try to built trivial Ethernet sample using MX (STM32CubeIDE/MX) it says me that LwIP cannot be attached if RTOS is not enabled - ?
Thanks Alexp
2019-09-11 6:06 AM
Why are You posting the same content twice?
Did You read the last sentence of my previous message? There are no publicly available quality STM32 ETH and lwIP driver code! Closest to usable is code from Keil DFP packs and ARM Mbed platform.
But if You need actually working network, then take this as an example and write Your own driver:
2019-09-11 6:58 AM
Hi Piranha,
1.Yes, I mistook and tried to delete one of two posts, but immediately get something similar ~"You Administrator closed this post and changing .*** ..."
Anyway Sorry(1);
2. Sorry(2) - I didn't understand firstly your sentence "P.S. Reliable, performant and compact lwIP examples fulfill only the 3rd point - they are invisible. " - I new user of ST and it my first project here (after TI)
=)
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.