cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP135f-dk USART synchronous mode support under Linux – CK signal not driven

Icyjkk
Visitor

Hello,

 

I am working with an STM32MP135f-dk device running Linux and trying to evaluate the possibility of using the USART peripheral in synchronous mode (TX/RX + CK).

 

From a hardware point of view, the STM32 USART clearly supports synchronous operation. However, when using the standard STM32 USART Linux kernel driver, the peripheral is only exposed as a /dev/ttySTM* device and operates strictly in asynchronous (UART) mode.

 

As far as I can see, the current driver does not enable or drive the CK clock signal, which makes true synchronous USART communication impossible under Linux, even though the underlying hardware is a USART.

 

My questions are:

1. Is this limitation expected by design in the current STM32 Linux USART driver?

 

2. Has anyone successfully implemented synchronous USART on STM32 under Linux, for example by: Extendimg the existing driver, writing a custom kernel driver, or using an alternative ?

1 REPLY 1
mfgkw
Senior III

Regarding 1.: yes

/dev/tty* seem to support only async mode, see https://wiki.st.com/stm32mpu/wiki/USART_internal_peripheral "4. Software frameworks and drivers":

Linux®: serial/tty framework; however, the Linux® kernel supports only the UART Asynchronous mode (Synchronous mode not supported)

 

So another driver will be required...