cancel
Showing results for 
Search instead for 
Did you mean: 

HTTP request to STM32 + LwIP results that Ping stops working

DMårt
Lead

Hello!

Recently I had problems with ping to my STM32 + LwIP + DP83848 + RMII. But the latest FW version 1.27.1, it works very well! But now I have problems with HTTP. Follow me and I show you how to create this bug.

First of all I'm using:

  • STM32CubeIDE 1.10.1
  • STM32F407VGT
  • FW 1.27.1

To reproduce this bug, do the following steps.

  • Step 1: Enable RMII by going to ETH -> RMII (Rx Buffer length 1524, MAC address 00:80:E1:00:00:00, Rx Mode = Interrupt, NVIC settings = Ethernet Global Interrupt)
  • Step 2: Go to FREERTOS and enable CMSIS V2 and go to Task & Queues. Change the Stack Size (Words) in defaultTask from 128 to 1024.
  • Step 3: Inside CMSIS V2, go to Advanced settings and set USE_NEWLIB_REENTRANT = Enabled. Leave everything else as default.
  • Step 4: Go to LWIP and enable it. Set LWIP_DHCP = disabled in General Settings and then write in the fixed IP address. In my case it is 192.168.1.35.
  • Step 5: Inside LWIP, go to HTTPD and set LWIP_HTTPD = enabled. Inside LWIP go to Key Options and set MEM_SIZE = 10*1024. Leave everything else as default.
  • Step 6: Download the FSDATA.zip folder and extract it.
  • Step 7: The FSDATA.zip folder contains a folder called FS and makeFSdata.exe. The makeFSdata.exe file will create a file called fsdata.c. Click on that.
  • Step 8: When the makeFSdata.exe file have created fsdata.c then rename fsdata.c to fsdata_custom.c.
  • Step 9: Place fsdata_custom.c at \Middlewares\Third_Party\LwIP\src\apps
  • Step 10: Right click fsdata_custom.c -> Resource Configurations -> Extract From Build ... -> Select All -> OK.
  • Step 11: Compile the project to your STM32 board and then ping.

0693W00000QN3y9QAD.png 

OK! It Working great!

  • Step 12: Download HTTP_Server.zip and extract it into the projects src folder.
  • Step 13: Write this into your main.c file
#include "HTTP_Server/httpserver.h"
  • Step 14: Add http_server_init(); to
/* USER CODE BEGIN Header_StartDefaultTask */
/**
  * @brief  Function implementing the defaultTask thread.
  * @param  argument: Not used
  * @retval None
  */
/* USER CODE END Header_StartDefaultTask */
void StartDefaultTask(void *argument)
{
  /* init code for LWIP */
  MX_LWIP_Init();
  /* USER CODE BEGIN 5 */
  http_server_init();
  /* Infinite loop */
  for(;;)
  {
    osDelay(1);
  }
  /* USER CODE END 5 */
}
  • Step 15: Compile and go to your web browser and type in 192.168.1.35/index.html. No web site is displayed. Also if I ping now, then I get no response....BUT....if I restart the processor, then ping, the ping is working. But as long I don't go to the 192.168.1.35/index.html website, my STM32 processor have connection to the DHCP server and I can ping it.

Question:

Why does this happen?

I have followed this tutorial 100% (except that he are using another processor) https://www.youtube.com/watch?v=haO8_eLIDeI&ab_channel=ControllersTech

This must be a bug, becase in FW 1.27.0 version, I had problems with ping my processor. In FW 1.27.1, the ping works like a charm. But now FW 1.27.1 resulting that my HTTPD won't work.

Thank you.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer
47 REPLIES 47

Hi @Daniel Mårtensson​ ,

>>> Where is the const data type?

In httpserver.c file (lines 32, 35, 42) remove the keyword "const" .

>>> When will ST implement this bug fix in next STCubeMXIDE?

It will be implemented in the next maintenance release for F4 planned on 23W24.

Regards

Mahdy

Is 23W24 weeks or a date? Like 23:e week 24? I did not understand "23W24".

Thank you so much.

Week 24 in 2023. June.

Sorry. I have no httpserver.c file in my project. I have enabled the HTTPD in CubeMX.

Hi. Sorry. Did not understand what you mean, but now I understand. I found the httpserver.c file. I removed the const data type, but it was the same issue as before. The ping stops working after I connect with my webbrowser to my ST processor.

Hi,

In order to reproduce your case with the same environment,

Could you please mention which CubeMX version you are using ?

Regards

Mahdy

I'm using STM32CubeIDE 1.10.1.

I'm asking about STM32CubeMX version (not STM32CubeIDE)

As mentioned below :

0693W00000Y7DYVQA3.pngGo to STM32CubeMX --> help --> About

I don't have STM32CubeMX. Only STM32CubeIDE.

Hi,

On the generated file "fsdata_custom.c" :

Http data are placed on flash and the Ethernet MAC does not have access to it.

So please replace it on RAM by removing the keyword "const" from lines :

28, 30, 103, 105, 168, 170, 308, 316 and 324.

Regards

Mahdy