‎2024-07-10 6:35 PM - edited ‎2024-07-10 6:36 PM
Hi,
I tried to set up and use HPDMA with ADC on my Nucleo-H7S3L8,
but I have some questions about how to use it.
Attached is the ADC_SingleConversion_TriggerSW_HPDMA example.
Solved! Go to Solution.
‎2024-08-08 7:16 PM
Hi @CMYL
Your code for regular DMA cannot be used with GPDMA and HPDMA.
I successfully ran Continuous Conversion Mode and DMA Circular Mode after enabling HPDMA and ADC in CubeMX.
Based on my debugging experience, the following points are key (though they might not be entirely correct).
My method is not a very good one; I found your GPDMA tutorial.
https://rristm.github.io/tomas_materials_v2/RRISTM/stm32u5_workshop/master
I followed the link-list setup in the tutorial, but it didn't work.One important reason is that the U5 only has one project, while the H7S3 has two: BOOT and APPLI.Maybe you should release an HPDMA tutorial for the H7S3.
‎2024-08-06 8:12 AM
Hello @prometheans152,
I agree with you HAL_ADC_Start is not mandatory we need only HAL_ADC_Start_DMA().
To configure the ADC in DMA Circular mode along with Continuous Conversion mode for 9 ADC channels, follow these steps:
Initialize the ADC:
ContinuousConvMode
to ENABLE
.ConversionDataManagement
to ADC_CONVERSIONDATA_DMA_CIRCULAR
.Configure the DMA:
Start the ADC with DMA:
HAL_ADC_Start_DMA
function to start the ADC in DMA mode.Here is a sample code snippet to illustrate the configuration:
#include "main.h"
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
#define ADC_CONVERTED_DATA_BUFFER_SIZE 9
uint32_t aADCxConvertedData[ADC_CONVERTED_DATA_BUFFER_SIZE];
void ADC_Init(void)
{
// Initialize the ADC handle
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE; // Enable scan mode for multiple channels
hadc1.Init.ContinuousConvMode = ENABLE; // Enable continuous conversion mode
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 9; // Number of conversions
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR; // Set DMA circular mode
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
// Initialization Error
Error_Handler();
}
// Configure the ADC channels
ADC_ChannelConfTypeDef sConfig = {0};
for (uint32_t i = 0; i < 9; i++)
{
sConfig.Channel = ADC_CHANNEL_0 + i; // Assuming channels 0 to 8
sConfig.Rank = ADC_REGULAR_RANK_1 + i;
sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
// Channel Configuration Error
Error_Handler();
}
}
}
void DMA_Init(void)
{
// Initialize the DMA handle
__HAL_RCC_DMA1_CLK_ENABLE();
hdma_adc1.Instance = DMA1_Channel1;
hdma_adc1.Init.Request = DMA_REQUEST_ADC1;
hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_adc1.Init.Mode = DMA_CIRCULAR; // Set DMA to circular mode
hdma_adc1.Init.Priority = DMA_PRIORITY_HIGH;
if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)
{
// Initialization Error
Error_Handler();
}
__HAL_LINKDMA(&hadc1, DMA_Handle, hdma_adc1);
}
void Start_ADC_DMA(void)
{
if (HAL_ADC_Start_DMA(&hadc1, (uint32_t *)aADCxConvertedData, ADC_CONVERTED_DATA_BUFFER_SIZE) != HAL_OK)
{
// Start Error
Error_Handler();
}
}
int main(void)
{
HAL_Init();
SystemClock_Config();
ADC_Init();
DMA_Init();
Start_ADC_DMA();
while (1)
{
// Main loop
}
}
‎2024-08-08 7:16 PM
Hi @CMYL
Your code for regular DMA cannot be used with GPDMA and HPDMA.
I successfully ran Continuous Conversion Mode and DMA Circular Mode after enabling HPDMA and ADC in CubeMX.
Based on my debugging experience, the following points are key (though they might not be entirely correct).
My method is not a very good one; I found your GPDMA tutorial.
https://rristm.github.io/tomas_materials_v2/RRISTM/stm32u5_workshop/master
I followed the link-list setup in the tutorial, but it didn't work.One important reason is that the U5 only has one project, while the H7S3 has two: BOOT and APPLI.Maybe you should release an HPDMA tutorial for the H7S3.
‎2024-08-09 2:55 AM
Hello @prometheans152
Sorry, I didn't pay attention that GPDMA/HPDMA is used. The H7S/R series has only GPDMA versus DMA in H7xx series.
Let me notice the difference in circular mode programming between GPDMA/HPDMA (General Purpose DMA) and DMA (Direct Memory Access).
Thanks for giving the solution :)
I highlight the workshop reference for community on STM32U5 GPDMA / LPBAM / ULP modes: https://rristm.github.io/tomas_materials_v2/RRISTM/stm32u5_workshop/master
Best regards,
‎2024-08-10 4:44 AM
Hi @CMYL
I think there are many deficiencies in your information about the H7S3 HPDMA.
The main points are as follows:
I believe your intention to introduce new technology is good, but could you please ensure everything is well-prepared before launching? This isn't the video game industry, where release debugging is acceptable.
‎2024-08-11 5:24 PM
Hello @prometheans152
Sorry I missed a last comment in my last message above: " I'm working on a project for Continuous Conversion Mode and DMA Circular Mode based on HPDMA, I will share it with you".
Note that for H7S series you need to focus on Appli project and use the boot project as provided by CubeMx for the Nucleo-H7S. Otherwise, I will share with you also the Howto for running and debugging your usecase.
For your third comment: ( 3. The examples are incomplete and contain errors.)
Otherwise, all the official documentations required to launch the product are available (STM32H7R7/7S7 - PDF Documentation:( RM0477, ANs, datasheets and ES .... HPDMA for example is detailed in chapter 13 of RM0477.
Best regards
‎2024-08-15 2:25 PM - edited ‎2024-08-15 2:26 PM
I deeply reviewed your questions. Here the answers to questions 1 and 2.
(I keep the answers to 3 and 4 in the next prompt window.)
//hadc1.Init.ContinuousConvMode = DISABLE; // --> ENABLE
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
Thanks
‎2024-08-15 4:41 PM
Hi,
For the following questions 3 and 4 below:
Answers:
- Please find my Step -by-Step demo in the attached document ADC_DMA_circular_usingSTM32CubeMx.pdf
- For the setting of STM32CubeIDE to avoid loading the boot binary each time you want to debug see attached document H7S_CubeIDE_config_Howto - Copy.pdf
- The whole project is attached ADC1_HPDMA_CircularMode.zip
Best Regards,
Younes