2024-07-08 07:24 AM
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file ux_device_msc.c
* @author MCD Application Team
* @brief USBX Device applicative file
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "ux_device_msc.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
#include "main.h"
#include "fx_stm32_sd_driver.h"
/* USER CODE END Includes */
#include "fx_api.h"
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
enum {
SD_WRITE_FLAG = 0x01,
SD_READ_FLAG = 0x02,
};
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
extern SD_HandleTypeDef hsd1;
extern HAL_SD_CardInfoTypeDef sd_info;
extern TX_EVENT_FLAGS_GROUP sdmmc_event;
extern FX_MEDIA sdio_disk;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
static INT check_sd_status(uint32_t instance)
{
uint32_t start = tx_time_get();
while (tx_time_get() - start < 100) {
if (fx_stm32_sd_get_status(instance) == 0) {
return 0;
}
}
return 1;
}
/* USER CODE END 0 */
/**
* @brief USBD_STORAGE_Activate
* This function is called when insertion of a storage device.
* @PAram storage_instance: Pointer to the storage class instance.
* @retval none
*/
VOID USBD_STORAGE_Activate(VOID *storage_instance)
{
/* USER CODE BEGIN USBD_STORAGE_Activate */
UX_PARAMETER_NOT_USED(storage_instance);
printf("USBD_STORAGE_Activate\n");
/* USER CODE END USBD_STORAGE_Activate */
return;
}
/**
* @brief USBD_STORAGE_Deactivate
* This function is called when extraction of a storage device.
* @PAram storage_instance: Pointer to the storage class instance.
* @retval none
*/
VOID USBD_STORAGE_Deactivate(VOID *storage_instance)
{
/* USER CODE BEGIN USBD_STORAGE_Activate */
UX_PARAMETER_NOT_USED(storage_instance);
printf("USBD_STORAGE_Activate\n");
/* USER CODE END USBD_STORAGE_Activate */
return;
}
/**
* @brief USBD_STORAGE_Read
* This function is invoked to read from media.
* @PAram storage_instance : Pointer to the storage class instance.
* @PAram lun: Logical unit number is the command is directed to.
* @PAram data_pointer: Address of the buffer to be used for reading or writing.
* @PAram number_blocks: number of sectors to read/write.
* @PAram lba: Logical block address is the sector address to read.
* @PAram media_status: should be filled out exactly like the media status
* callback return value.
* @retval status
*/
UINT USBD_STORAGE_Read(VOID *storage_instance, ULONG lun, UCHAR *data_pointer,
ULONG number_blocks, ULONG lba, ULONG *media_status)
{
UINT status = UX_SUCCESS;
/* USER CODE BEGIN USBD_STORAGE_Read */
UX_PARAMETER_NOT_USED(storage_instance);
UX_PARAMETER_NOT_USED(lun);
// UX_PARAMETER_NOT_USED(data_pointer);
// UX_PARAMETER_NOT_USED(number_blocks);
// UX_PARAMETER_NOT_USED(lba);
UX_PARAMETER_NOT_USED(media_status);
ULONG WriteFlags = 0;
status = UX_ERROR;
status = check_sd_status(0);
if (status) {
printf("SD card not ready\n");
return status;
}
/* Start the Dma write */
status = fx_stm32_sd_read_blocks(0, (UINT *)data_pointer, lba, number_blocks);
if(status != HAL_OK) {
printf("HAL_SD_ReadBlocks_DMA failed\n");
}
/* Wait on readflag until SD card is ready to use for new operation */
tx_event_flags_get(&sdmmc_event,
SD_READ_FLAG,
TX_OR_CLEAR,
&WriteFlags,
TX_WAIT_FOREVER);
/* USER CODE END USBD_STORAGE_Read */
return status;
}
/**
* @brief USBD_STORAGE_Write
* This function is invoked to write in media.
* @PAram storage_instance : Pointer to the storage class instance.
* @PAram lun: Logical unit number is the command is directed to.
* @PAram data_pointer: Address of the buffer to be used for reading or writing.
* @PAram number_blocks: number of sectors to read/write.
* @PAram lba: Logical block address is the sector address to read.
* @PAram media_status: should be filled out exactly like the media status
* callback return value.
* @retval status
*/
UINT USBD_STORAGE_Write(VOID *storage_instance, ULONG lun, UCHAR *data_pointer,
ULONG number_blocks, ULONG lba, ULONG *media_status)
{
UINT status = UX_SUCCESS;
/* USER CODE BEGIN USBD_STORAGE_Write */
UX_PARAMETER_NOT_USED(storage_instance);
// UX_PARAMETER_NOT_USED(lun);
// UX_PARAMETER_NOT_USED(data_pointer);
// UX_PARAMETER_NOT_USED(number_blocks);
// UX_PARAMETER_NOT_USED(lba);
UX_PARAMETER_NOT_USED(media_status);
ULONG ReadFlags = 0U;
status = UX_ERROR;
status = check_sd_status(0);
if (status) {
printf("SD card not ready\n");
return status;
}
/* Start the Dma write */
status = fx_stm32_sd_write_blocks(0, (UINT *)data_pointer, lba, number_blocks);
if(status != HAL_OK) {
printf("HAL_SD_WriteBlocks_DMA failed\n");
}
/* Wait on writeflag until SD card is ready to use for new operation */
tx_event_flags_get(&sdmmc_event,
SD_WRITE_FLAG,
TX_OR_CLEAR,
&ReadFlags,
TX_WAIT_FOREVER);
/* USER CODE END USBD_STORAGE_Write */
return status;
}
/**
* @brief USBD_STORAGE_Flush
* This function is invoked to flush media.
* @PAram storage_instance : Pointer to the storage class instance.
* @PAram lun: Logical unit number is the command is directed to.
* @PAram number_blocks: number of sectors to read/write.
* @PAram lba: Logical block address is the sector address to read.
* @PAram media_status: should be filled out exactly like the media status
* callback return value.
* @retval status
*/
UINT USBD_STORAGE_Flush(VOID *storage_instance, ULONG lun, ULONG number_blocks,
ULONG lba, ULONG *media_status)
{
UINT status = UX_SUCCESS;
/* USER CODE BEGIN USBD_STORAGE_Flush */
UX_PARAMETER_NOT_USED(storage_instance);
UX_PARAMETER_NOT_USED(lun);
UX_PARAMETER_NOT_USED(number_blocks);
UX_PARAMETER_NOT_USED(lba);
UX_PARAMETER_NOT_USED(media_status);
// status = UX_ERROR;
/* USER CODE END USBD_STORAGE_Flush */
return status;
}
/**
* @brief USBD_STORAGE_Status
* This function is invoked to obtain the status of the device.
* @PAram storage_instance : Pointer to the storage class instance.
* @PAram lun: Logical unit number is the command is directed to.
* @PAram media_id: is not currently used.
* @PAram media_status: should be filled out exactly like the media status
* callback return value.
* @retval status
*/
UINT USBD_STORAGE_Status(VOID *storage_instance, ULONG lun, ULONG media_id,
ULONG *media_status)
{
UINT status = UX_SUCCESS;
/* USER CODE BEGIN USBD_STORAGE_Status */
UX_PARAMETER_NOT_USED(storage_instance);
UX_PARAMETER_NOT_USED(lun);
UX_PARAMETER_NOT_USED(media_id);
UX_PARAMETER_NOT_USED(media_status);
// status = UX_ERROR;
/* USER CODE END USBD_STORAGE_Status */
return status;
}
/**
* @brief USBD_STORAGE_Notification
* This function is invoked to obtain the notification of the device.
* @PAram storage_instance : Pointer to the storage class instance.
* @PAram lun: Logical unit number is the command is directed to.
* @PAram media_id: is not currently used.
* @PAram notification_class: specifies the class of notification.
* @PAram media_notification: response for the notification.
* @PAram media_notification_length: length of the response buffer.
* @retval status
*/
UINT USBD_STORAGE_Notification(VOID *storage_instance, ULONG lun, ULONG media_id,
ULONG notification_class, UCHAR **media_notification,
ULONG *media_notification_length)
{
UINT status = UX_SUCCESS;
/* USER CODE BEGIN USBD_STORAGE_Notification */
UX_PARAMETER_NOT_USED(storage_instance);
UX_PARAMETER_NOT_USED(lun);
UX_PARAMETER_NOT_USED(media_id);
UX_PARAMETER_NOT_USED(notification_class);
UX_PARAMETER_NOT_USED(media_notification);
UX_PARAMETER_NOT_USED(media_notification_length);
// status = UX_ERROR;
/* USER CODE END USBD_STORAGE_Notification */
return status;
}
/**
* @brief USBD_STORAGE_GetMediaLastLba
* Get Media last LBA.
* @PAram none
* @retval last lba
*/
ULONG USBD_STORAGE_GetMediaLastLba(VOID)
{
ULONG LastLba = 0U;
/* USER CODE BEGIN USBD_STORAGE_GetMediaLastLba */
LastLba = (ULONG)(sd_info.BlockNbr - 1);
/* USER CODE END USBD_STORAGE_GetMediaLastLba */
return LastLba;
}
/**
* @brief USBD_STORAGE_GetMediaBlocklength
* Get Media block length.
* @PAram none.
* @retval block length.
*/
ULONG USBD_STORAGE_GetMediaBlocklength(VOID)
{
ULONG MediaBlockLen = 0U;
/* USER CODE BEGIN USBD_STORAGE_GetMediaBlocklength */
MediaBlockLen = (ULONG) sd_info.BlockSize;
/* USER CODE END USBD_STORAGE_GetMediaBlocklength */
return MediaBlockLen;
}
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
2024-07-08 09:14 AM - edited 2024-07-08 09:14 AM
filex_media_open() is not a standard function in the FileX stack or ST's stack. Instead, it seems to be a custom function. Could you provide more details about the function definition?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-08 09:23 AM
>USBX MSC cannot be used when using filex_media_open()
-- you mean: fx_media_open(..) ?
2024-07-08 04:20 PM
oh, i'm sorry fx_media_open() is right
void fx_app_thread_entry(ULONG thread_input)
{
UINT sd_status = FX_SUCCESS;
UINT nor_ospi_status = FX_SUCCESS;
/* USER CODE BEGIN fx_app_thread_entry 0*/
/* USER CODE END fx_app_thread_entry 0*/
/* Open the SD disk driver */
sd_status = fx_media_open(&sdio_disk, FX_SD_VOLUME_NAME, fx_stm32_sd_driver, (VOID *)FX_NULL, (VOID *) fx_sd_media_memory, sizeof(fx_sd_media_memory));
// /* Check the media open sd_status */
if (sd_status != FX_SUCCESS)
{
/* USER CODE BEGIN SD DRIVER get info error */
while(1);
/* USER CODE END SD DRIVER get info error */
}
/* Open the OCTO-SPI NOR driver */
nor_ospi_status = fx_media_open(&nor_ospi_flash_disk, FX_NOR_OSPI_VOLUME_NAME, fx_stm32_levelx_nor_driver, (VOID *)LX_NOR_OSPI_DRIVER_ID, (VOID *) fx_nor_ospi_media_memory, sizeof(fx_nor_ospi_media_memory));
/* Check the media open nor_ospi_status */
if (nor_ospi_status != FX_SUCCESS)
{
/* USER CODE BEGIN OCTO-SPI NOR open error */
while(1);
/* USER CODE END OCTO-SPI NOR open error */
}
/* USER CODE BEGIN fx_app_thread_entry 1*/
UINT status;
CHAR entry_name[256];
UINT attributes;
ULONG size;
UINT year;
UINT month;
UINT day;
UINT hour;
UINT minute;
UINT second;
/* Get the next directory entry in the default directory with full information. */
printf("nor flash disk directory:\n");
do {
status = fx_directory_next_full_entry_find(&nor_ospi_flash_disk, entry_name, &attributes, &size,
&year, &month, &day,
&hour, &minute, &second);
if (status == FX_SUCCESS) {
/* Process the directory entry. */
printf("File: %s, Size: %lu, Date: %02u/%02u/%04u, Time: %02u:%02u:%02u\n",
entry_name, size, day, month, year, hour, minute, second);
}
} while (status == FX_SUCCESS);
/* Get the next directory entry in the default directory with full information. */
printf("sd disk directory:\n");
do {
status = fx_directory_next_full_entry_find(&sdio_disk, entry_name, &attributes, &size,
&year, &month, &day,
&hour, &minute, &second);
if (status == FX_SUCCESS) {
/* Process the directory entry. */
printf("File: %s, Size: %lu, Date: %02u/%02u/%04u, Time: %02u:%02u:%02u\n",
entry_name, size, day, month, year, hour, minute, second);
}
} while (status == FX_SUCCESS);
status = fx_media_close(&sdio_disk);
if (status) {
printf("Failed to close sd disk: %x\n", status);
}
/* USER CODE END fx_app_thread_entry 1*/
}
2024-07-08 04:25 PM
oh, i'm sorry. fx_media_open () is correct. I added the code below.
2024-07-08 04:27 PM
oh, i'm sorry. fx_media_open () is correct. I added the code below~
2024-07-09 12:48 AM
One sorry is enough.. 🙂
> USBX MSC cannot be used when using filex_media_open().
In your code i see open for sd-card and nor-flash - so what about the usb problem ?