2023-02-08 10:56 AM
Hello,
I am a newcomer to the ST world- I am working with VW of America and UTK on a senior design project.
I am attempting to setup a USB-C PD source application using a NUCLEO-G491RE Connected to a SRC1M1 extension board. I have tried directly loading the src1M1 example project in x-cube-tcpp (nucleo-g474re/applications/USB_PD/SRC1M1_Source) and following this guide on the wiki. For the wiki project, I applied the correct BSP and adjusted the .extsettings file to point to the correct BSP.
When monitoring stcubemonitor-UCPD, neither stack seems to be responding in the desired manner, and no contract is negotiated.
What further steps should I be taking to set up my USB-C application? I know this is a desired function from ST, so it should be pretty simple.
2023-03-09 12:54 AM
How can you be sure you are really doing power delivery? Charging your device does not mean you exercise power delivery. Remember that 5V is type C basic, and so, from what I see from the trace do not confirm that you have request/ accept, and power delivery explicit contract.
Check this wiki