cancel
Showing results for 
Search instead for 
Did you mean: 

How to replicate the shutdown behavior with wake-up via double tap of the ALLMEMS1 firmware in AI-SENSING1 for SensorTile (STEVAL-STLKT01V1)

Emanuel_S
Visitor

Hello,

I'm working with SensorTile (STEVAL-STLKT01V1) and using the AI-SENSING1 firmware. I would like to replicate the energy saving behavior I observed in the ALLMEMS1 firmware: it goes into shutdown mode after a period of no connection and can be reactivated by a double tap event. In ALLMEMS1, this behavior happens automatically, but in AI-SENSING1, I am facing difficulties implementing this logic.

My question is: what specific steps should I follow to replicate the behavior of ALLMEMS1 in AI-SENSING1, or is there any example of implementing this shutdown with wake-up via double tap for AI-SENSING1? I would also need guidance on how to configure the timer so that the shutdown occurs automatically after a pre-determined time without connection.

Thanks in advance for any help or guidance.

0 REPLIES 0