2022-08-14 2:18 PM
Hello Community,
I'm working on stm32u5(B-U585I-IOT02A). B-U585I-IOT02A has two digital mics, and St officially has an example of BSP to record audio.
So after taking references from: https://github.com/STMicroelectronics/STM32CubeU5/blob/main/Projects/B-U585I-IOT02A/Examples/BSP/Src/audio_record.c
I've started the project but I'm getting issues with initializing BSP_AUDIO_IN_Init(0, &AudioInit), when I'm calling this function I'm getting: bsp_error_periph_failure(-4)
I don't know where I'm lagging can anyone provide me a solution to fix this error?
I really appreciate any help you can provide.
2022-08-16 1:36 AM
Hi @radeshsharma ,
Can you check that you are using the right microphone (AUDIO_IN_DEVICE_DIGITAL 1 OR 2)? And that it is connected to the right place?
Regards,
DianeP
2022-08-26 12:48 PM
Hello @Diane POMABIA
Thanks for your response. I was using AUDIO_IN_DEVICE_DIGITAL_MIC1 it was throwing bsp_error_periph_failure(-4), but after changing it to AUDIO_IN_DEVICE_DIGITAL_MIC2 it didn't throw any error but still, the recording didn't start. I tried to debug it. So, I tried to run the code line by line and I got to know things were becoming no response after reaching inside int32_t BSP_AUDIO_IN_Record(uint32_t Instance, uint8_t *pData, uint32_t NbrOfBytes)--> HAL_MDF_AcqStart_DMA(&haudio_in_mdf_filter[1], &filterConfig, &dmaConfig) --> MDF_AcqStart(hmdf, pFilterConfig); at this point code doesn't response anything, didn't throw any error just go loop.
Do you have any suggestions on this?