2022-02-24 12:53 AM
Hello everyone,
I have a custom board based on X-CUBE-AZURE, connecting and sending data to a our own Azure Server. When connecting a device we get security alerts from Azure, telling that we do not use a TLS certificate validation. I have found in my software where to put the certificate, but I have to generate it in .pem file from Azure.
Do you have any idea or any documentation about how to do that ? Thanks in advance
2022-02-24 10:27 AM
Hello
which certificate are you talking of ? is it a device certificate ? or Azure IoT server root certificate ?
the Azure root certificates are available in https://github.com/Azure/azure-iot-sdk-c/blob/main/certs/certs.c
2022-02-24 10:57 PM
Hello Guillaume and thank you for your answer.
As I have no experience in IoT security I do not really know, the alert message I received is : IoT devices running C-SDK + OpenSSL/WolfSSL perform no validation of the remote TLS server certificate.
After some research I have found that there is a certificate in the file iot_flash_config.c, in the function CaptureAndFlashPem(). Originnally it requests the user to give a string array, but in my case the string array is hardcoded in the function, instead to request it. Let me precise that this part has not been made by me. I have discussed with the person in charge of this and he told me he get this certificate from ST.
int CaptureAndFlashPem(char *pem_name, char const *flash_addr, bool restricted_area)
{
char * key_read_buffer = NULL;
int ret = 0;
key_read_buffer="-----BEGIN CERTIFICATE-----\nMIIF3jCCA8agAwIBAgIQAf1tMPyjylGoG7xkDjUDLTANBgkqhkiG9w0BAQwFADCB\n"
"iDELMAkGA1UEBhMCVVMxEzARBgNVBAgTCk5ldyBKZXJzZXkxFDASBgNVBAcTC0pl\ncnNleSBDaXR5MR4wHAYDVQQKExVUaGUgVVNFUlRSVVNUIE5ldHdvcmsxLjAsBgNV\n"
"BAMTJVVTRVJUcnVzdCBSU0EgQ2VydGlmaWNhdGlvbiBBdXRob3JpdHkwHhcNMTAw\nMjAxMDAwMDAwWhcNMzgwMTE4MjM1OTU5WjCBiDELMAkGA1UEBhMCVVMxEzARBgNV\n"
"BAgTCk5ldyBKZXJzZXkxFDASBgNVBAcTC0plcnNleSBDaXR5MR4wHAYDVQQKExVU\naGUgVVNFUlRSVVNUIE5ldHdvcmsxLjAsBgNVBAMTJVVTRVJUcnVzdCBSU0EgQ2Vy\n"
"dGlmaWNhdGlvbiBBdXRob3JpdHkwggIiMA0GCSqGSIb3DQEBAQUAA4ICDwAwggIK\nAoICAQCAEmUXNg7D2wiz0KxXDXbtzSfTTK1Qg2HiqiBNCS1kCdzOiZ/MPans9s/B\n"
"3PHTsdZ7NygRK0faOca8Ohm0X6a9fZ2jY0K2dvKpOyuR+OJv0OwWIJAJPuLodMkY\ntJHUYmTbf6MG8YgYapAiPLz+E/CHFHv25B+O1ORRxhFnRghRy4YUVD+8M/5+bJz/\n"
"Fp0YvVGONaanZshyZ9shZrHUm3gDwFA66Mzw3LyeTP6vBZY1H1dat//O+T23LLb2\nVN3I5xI6Ta5MirdcmrS3ID3KfyI0rn47aGYBROcBTkZTmzNg95S+UzeQc0PzMsNT\n"
"79uq/nROacdrjGCT3sTHDN/hMq7MkztReJVni+49Vv4M0GkPGw/zJSZrM233bkf6\nc0Plfg6lZrEpfDKEY1WJxA3Bk1QwGROs0303p+tdOmw1XNtB1xLaqUkL39iAigmT\n"
"Yo61Zs8liM2EuLE/pDkP2QKe6xJMlXzzawWpXhaDzLhn4ugTncxbgtNMs+1b/97l\nc6wjOy0AvzVVdAlJ2ElYGn+SNuZRkg7zJn0cTRe8yexDJtC/QV9AqURE9JnnV4ee\n"
"UB9XVKg+/XRjL7FQZQnmWEIuQxpMtPAlR1n6BB6T1CZGSlCBst6+eLf8ZxXhyVeE\nHg9j1uliutZfVS7qXMYoCAQlObgOK6nyTJccBz8NUvXt7y+CDwIDAQABo0IwQDAd\n"
"BgNVHQ4EFgQUU3m/WqorSs9UgOHYm8Cd8rIDZsswDgYDVR0PAQH/BAQDAgEGMA8G\nA1UdEwEB/wQFMAMBAf8wDQYJKoZIhvcNAQEMBQADggIBAFzUfA3P9wF9QZllDHPF\n"
"Up/L+M+ZBn8b2kMVn54CVVeWFPFSPCeHlCjtHzoBN6J2/FNQwISbxmtOuowhT6KO\nVWKR82kV2LyI48SqC/3vqOlLVSoGIG1VeCkZ7l8wXEskEVX/JJpuXior7gtNn3/3\n"
"ATiUFJVDBwn7YKnuHKsSjKCaXqeYalltiz8I+8jRRa8YFWSQEg9zKC7F4iRO/Fjs\n8PRF/iKz6y+O0tlFYQXBl2+odnKPi4w2r78NBc5xjeambx9spnFixdjQg3IM8WcR\n"
"iQycE0xyNN+81XHfqnHd4blsjDwSXWXavVcStkNr/+XeTWYRUc+ZruwXtuhxkYze\nSf7dNXGiFSeUHM9h4ya7b6NnJSFd5t0dCy5oGzuCr+yDZ4XUmFF0sbmZgIn/f3gZ\n"
"XHlKYC6SQK5MNyosycdiyA5d9zZbyuAlJQG03RoHnHcAP9Dc1ew91Pq7P8yF1m9/\nqS3fuQL39ZeatTXaw2ewh0qpKJ4jjv9cJ2vhsE/zB+4ALtRZh8tSQZXq9EfX7mRB\n"
"VXyNWQKV3WKdwrnuWih0hKWbt5DHDAff9Yk2dDLWKMGwsAvgnEzDHNb842m1R0aB\nL6KCq9NjRHDEjf8tM7qtj3u1cIiuPhnPQCjY/MiQu12ZIvVS5ljFH4gxQ+6IHdfG\n"
"jjxDah2nGN59PRbxYvnKkKj9\n-----END CERTIFICATE-----\n-----BEGIN CERTIFICATE-----\n"
"MIIDdzCCAl+gAwIBAgIEAgAAuTANBgkqhkiG9w0BAQUFADBaMQswCQYDVQQGEwJJ\nRTESMBAGA1UEChMJQmFsdGltb3JlMRMwEQYDVQQLEwpDeWJlclRydXN0MSIwIAYD\n"
"VQQDExlCYWx0aW1vcmUgQ3liZXJUcnVzdCBSb290MB4XDTAwMDUxMjE4NDYwMFoX\nDTI1MDUxMjIzNTkwMFowWjELMAkGA1UEBhMCSUUxEjAQBgNVBAoTCUJhbHRpbW9y\n"
"ZTETMBEGA1UECxMKQ3liZXJUcnVzdDEiMCAGA1UEAxMZQmFsdGltb3JlIEN5YmVy\nVHJ1c3QgUm9vdDCCASIwDQYJKoZIhvcNAQEBBQADggEPADCCAQoCggEBAKMEuyKr\n"
"mD1X6CZymrV51Cni4eiVgLGw41uOKymaZN+hXe2wCQVt2yguzmKiYv60iNoS6zjr\nIZ3AQSsBUnuId9Mcj8e6uYi1agnnc+gRQKfRzMpijS3ljwumUNKoUMMo6vWrJYeK\n"
"mpYcqWe4PwzV9/lSEy/CG9VwcPCPwBLKBsua4dnKM3p31vjsufFoREJIE9LAwqSu\nXmD+tqYF/LTdB1kC1FkYmGP1pWPgkAx9XbIGevOF6uvUA65ehD5f/xXtabz5OTZy\n"
"dc93Uk3zyZAsuT3lySNTPx8kmCFcB5kpvcY67Oduhjprl3RjM71oGDHweI12v/ye\njl0qhqdNkNwnGjkCAwEAAaNFMEMwHQYDVR0OBBYEFOWdWTCCR1jMrPoIVDaGezq1\n"
"BE3wMBIGA1UdEwEB/wQIMAYBAf8CAQMwDgYDVR0PAQH/BAQDAgEGMA0GCSqGSIb3\nDQEBBQUAA4IBAQCFDF2O5G9RaEIFoN27TyclhAO992T9Ldcw46QQF+vaKSm2eT92\n"
"9hkTI7gQCvlYpNRhcL0EYWoSihfVCr3FvDB81ukMJY2GQE/szKN+OMY3EU/t3Wgx\njkzSswF07r51XgdIGn9w/xZchMB5hbgF/X++ZRGjD8ACtPhSNzkE1akxehi/oCr0\n"
"Epn3o0WC4zxe9Z2etciefC7IpJ5OCBRLbf1wbWsaY71k5h+3zvDyny67G7fyUIhz\nksLi4xaNmjICq44Y3ekQEe5+NauQrz4wlHrQMz2nZQ/1/I6eYs9HRCwBXbsdtTLS\n"
"R9I4LtD+gdwyah617jzV/OeBHRnDJELqYzmp\n-----END CERTIFICATE-----\n\0";
/* Write to Flash. */
TRACE_FLASH("writing to %lx\n", flash_addr);
ret = FLASH_update((uint32_t)flash_addr, key_read_buffer, strlen(key_read_buffer) + 1); /* Append the closing \0*/
//free(key_read_buffer);
return ret;
}
So, I have a certificate on Azure app service :
I would like to know how to add it in my code. It seems I have to download it in .pem format but I do not know how to do it.
Thank you
2022-02-25 09:18 AM
This is confusing. X-CUBE-AZURE purpose is to connect an IoT device to an Azure IoT Hub.
You are talking about an Azure App Service certificate. So it is not the same thing .
Going back to the original problem, what is the exact warning message from Azure ? ("When connecting a device we get security alerts from Azure, telling that we do not use a TLS certificate validation.")
is it written exactly like this ?
I know the root CA certificates from Azure will change soon. Is it this specific problem ?
https://docs.microsoft.com/en-us/azure/security/fundamentals/tls-certificate-changes
2022-02-27 10:57 PM
Sorry for being confusing, maybe I will go too fast.
The original alert message received by Azure is:
Issue
IoT devices running C-SDK + OpenSSL/WolfSSL perform no validation of the remote TLS server certificate. The security advisory is present both in our GitHub Repo as well as CVE-2020-17002.
Affected versions:
<2020-12-09, <LTS_07_2020_Ref02, <LTS_02_2020_Ref02, Public-Preview <1.6.0
Patched versions:
2020-12-09, LTS_07_2020_Ref02, LTS_02_2020_Ref02, Public-Preview 1.6.0
Recommended actions:
Update all impacted devices to patched versions.
Security reminder:
Continuously monitor Azure IoT CVEs for other Azure IoT security related issues
2022-02-28 12:45 AM
As far as I understand the problem is not with the certificate itself. It's the software used for TLS communication that doesn't use the certificate.
The security article mentions WolfSSL and OpenSSL. But X-CUBE-AZURE uses mbedTLS. So are you using a modified X-CUBE-AZURE or an entirely different software ?
2022-02-28 12:50 AM
I am using a project based on X-CUBE-AZURE, with changes on application layer only. I agree with you on the fact it uses mbedTLS, I already have seen in debug mode that it goes in mbedTLS files.