2022-03-28 12:13 PM
I try to create a new project, nothing is written in main.c! It is a first check after setting up 'LWIP', 'SDIO' and Freertos in the GUI and got this mistake!
multiple definition of `errno'; ./Middlewares/Third_Party/LwIP/system/OS/sys_arch.o:/home/denis/STM32CubeIDE/workspace_1.9.0/FreeRtos_SDIO_Web/Debug/../Middlewares/Third_Party/LwIP/system/OS/sys_arch.c:45: first defined here
STM32CubeIDE Version: 1.9.0
PS - This error not appear then I was on STM32CubeIDE Version: 1.8.0
Solved! Go to Solution.
2022-04-11 3:14 AM
2022-03-28 12:17 PM
>>How to fix "multiple definition of `errno"'?
Remove all but one? Make some weak?
Make sure multiple instances of the same object aren't pulled in
2022-03-28 12:44 PM
The file "sys_arch.o" is not readable.
And if I will comment three lines in the file sys_arch.c is it will correct?
I'm asking because according to the error /Middlewares/Third_Party/LwIP/system/OS/sys_arch.c:45: first defined here
2022-03-28 12:46 PM
2022-03-28 12:58 PM
Thanks for the link! But, in my case, I have nothing in main.c and there is nothing in headers files and so on. It is a first check after setting up in GUI what I do wrong or how it is fix?
2022-03-28 1:32 PM
If you're using the ST toolchain, errno is defined by its C library (newlib).
So just #include <errno.h> ; remove all other definitions of errno,
2022-03-28 1:38 PM
From the thread I linked to:
> ... use -fcommon to compile ...
JW
2022-03-28 1:45 PM
Is it correct?
2022-03-28 1:47 PM
Could you please make screen? Because I don't understand what you are mean...
2022-03-28 1:57 PM
Or remove the command line define LWIP_PROVIDE_ERRNO, or have it called out as "extern"
Evidently the devs have previously had just this issue.
Pretty sure using "extern" would have all secondary references fold into one.