2022-06-22 11:53 PM
I tried activating the sim from the module P-L496G-CELL01 as the link was redirecting to the home and another link was redirecting to the second version of the module. Is there a way to activate the sim? Is there a way to upgrade the first hardware firmware to the second version or should I buy the second module.
2022-06-23 02:58 AM
Please check the followong thread, but don't know whether it works with P-L496G-CELL01:
https://www.st.com/resource/en/utilities/p-l496g-cell02_sim_mmf2.zip
@Ronan GABOU
2022-06-23 08:39 PM
Hi Mike
The firmware version of cell 01 is different from the cell 02. I went through the above query, the links provided in the query has been expired and also the instruction from cell 02 doesn't work with cell 01 as the instructions and the start menu are different. Is there a way to work around that or shall I upgrade the firmware and If its possible to upgrade the firmware can you please provide the necessary files and instructions to it.
2022-06-24 01:20 AM
@Seb
2022-06-27 08:07 PM
Hey!
Is there any update?