2021-10-11 04:22 PM
Using B-L462E-CELL1 with X-CUBE-CELLULAR 6.01 and I have adapted one of the cellular apps using cellular_app_socket_obtain() to connect, and cellular_app_socket_close() to close a socket. The server connection initially succeeds, but after the remote server is bounced manually as a test, the socket is closed and a new socket is obtained. However the connection to the server keeps failing.
2021-10-12 11:16 AM
See attached logs
2021-10-29 10:58 AM
Dear JVand.12
Can you share the log to better understanding the issue you are facing?
Thanks a lot
Best Regards
Solofo